Question
ADC initialization error. USART conflict?
Posted on December 10, 2014 at 23:04
Hello,
I'm trying to initialize my ADC to continuously sample, but I must have overlooked something since I'm stuck when waiting for ADC_FLAG_ADONS. I'm programming to the STM32L152C Discovery board, but want to move my code to theSTM32L151CBT6
when I've confirmed the functionality. I'm also using port A as a USART port, does this conflict in setting up the ADC? I cannot find anything suggesting it, but as I said, I might have overlooked some detail. The last thing on the serial port to come out is ''a1''. Code snippets:
void
Init_RCC()
{
/* Enable MSI and wait for it to be ready.
* The Cmd call is implicty since it restarts after every board reset.
*/
RCC_MSICmd(ENABLE);
while
(RCC_GetFlagStatus(RCC_FLAG_MSIRDY) == RESET);
/* Allow access to the RTC */
PWR_RTCAccessCmd(ENABLE);
/* LSE Enable */
RCC_LSEConfig(RCC_LSE_ON);
/* Wait until LSE is ready */
while
(RCC_GetFlagStatus(RCC_FLAG_LSERDY) == RESET);
/* Reset RCC */
RCC_DeInit();
/* Set MSI as SYSCLOCK */
RCC_SYSCLKConfig(RCC_SYSCLKSource_MSI);
//MSI
/* Setting the SYSCLOCK frequency */
RCC_MSIRangeConfig(RCC_MSIRange_6);
// Range_6 = 4.194MHz
/* Enable GPIO port B (contains LEDs) */
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOB, ENABLE);
/* Allow access to the RTC */
PWR_RTCAccessCmd(ENABLE);
/* Reset RTC Backup Domain */
RCC_RTCResetCmd(ENABLE);
RCC_RTCResetCmd(DISABLE);
/* RTC Clock Source Selection */
RCC_RTCCLKConfig(RCC_RTCCLKSource_LSE);
/* Enable the RTC */
RCC_RTCCLKCmd(ENABLE);
RCC_MSICmd(ENABLE);
}
void
Init_ADC()
{
GPIO_InitTypeDef GPIO_InitStruct;
ADC_InitTypeDef ADC_InitStructure;
/* GPIO Init. Set PA5 as analog input*/
GPIO_InitStruct.GPIO_Pin = GPIO_Pin_5;
GPIO_InitStruct.GPIO_Mode = GPIO_Mode_AN;
GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_Init(GPIOA, &GPIO_InitStruct);
/* ADC Init. */
RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1, ENABLE);
ADC_DeInit(ADC1);
ADC_StructInit(&ADC_InitStructure);
ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b;
ADC_InitStructure.ADC_ScanConvMode = ENABLE;
ADC_InitStructure.ADC_ContinuousConvMode = ENABLE;
// ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None;
//ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_T9_TRGO; // Trigger on timer 9 update event
//ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;
ADC_InitStructure.ADC_NbrOfConversion = 1;
ADC_Init(ADC1, &ADC_InitStructure);
ADC_PowerDownCmd(ADC1, ADC_PowerDown_Idle_Delay, ENABLE);
/* Enable ADC1 */
ADC_Cmd(ADC1, ENABLE);
/* Wait until ADC1 ON status */
printText(
''a1''
);
/* Wait until ADC1 ON status */
while
(ADC_GetFlagStatus(ADC1, ADC_FLAG_ADONS) == RESET)
{
}
printText(
''a222''
);
}
void
Init_USART1(
void
)
{
GPIO_InitTypeDef GPIO_InitStructure;
USART_InitTypeDef USART_InitStructure;
/* Enable bus clocks */
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);
RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1, ENABLE);
/* Set USART1 Tx (PA.09) as AF push-pull */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_40MHz;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_Init(GPIOA, &GPIO_InitStructure);
/* Set USART1 Rx (PA.10) as input floating */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_Init(GPIOA, &GPIO_InitStructure);
/* Attach Pin 9 and 10 to USART port */
GPIO_PinAFConfig(GPIOA, GPIO_PinSource10, GPIO_AF_USART1);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource9, GPIO_AF_USART1);
/* Initialize USART parameters */
USART_InitStructure.USART_BaudRate = 9600;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_No ;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
USART_Init(USART1, &USART_InitStructure);
USART_Cmd(USART1, ENABLE);
}
void
printText(
char
* t)
{
uint8_t i = 0;
for
( i = 0; i<strlen(t); i++ )
{
Usart1Put(t[i]);
}
}
int
main(
void
)
{
Init_RCC();
Init_USART1();
Init_LEDs();
printText(
''main1''
);
Init_Timer10();
printText(
''main2''
);
Init_Timer11();
printText(
''main3''
);
Init_ADC();
printText(
''main4''
);
Init_TimerInterrupt();
printText(
''main6''
);
while
(1)
{
// Do it forever
}
}
#stm32-adc-timer-initialization