Question
Uart variable length
Posted on December 20, 2015 at 14:56
Hi !
I need to implement a Rx-uart at 250k bauds with variable length but the problem is that I'm with the CubeMX configurator and I don't know how to do it.I was also trying to receive the data in DMA but when I call HAL_UART_Receive_DMA, I receive a 0x00 at the first byte but when I call HAL_UART_Receive_IT at the same place, I receive the byte I need. (0xCC)If someone can help me... Here is some code :void HAL_TIM_IC_CaptureCallback(TIM_HandleTypeDef *htim){ if (htim->Instance==TIM2) { if(HAL_TIM_ReadCapturedValue(&htim2,TIM_CHANNEL_2) >= 176) { HAL_UART_Receive_DMA(&huart1,data_rdm_discovery,38); } } } /*when I have a break of 176 us I call HAL_UART_Receive_DMA(&huart1,data_rdm_discovery,38)*/Then I analyze the packet with the rxcplt_callback #hal #uart #!stm32 #stmf1