STM32F7 ethernet issues in RMII mode
I have a STM32F767 and STM32F746 nucleo dev kits. Both seems to be 'Z' models.
I developed RTOS based TCP server based on netconn that receives and transmits data over ethernet. STM does not answer to the ping nor sending/receiving any data. On the ethernet plug both green and yello LEDs are on. Problem is that after several restarts ethernet starts working until the next restart, if I am lucky. I have noticed that eth works only when green LED is off on the ethernet plug.
At first I thought problem is on my SW side. I developed similar server using RAW sockets, then tried with UDP client - same issues.
At first I tried with STM32F767 but then replaced it with STM32F746 just for testing purposes - still same issues.
Reading errata sheets I saw similar problems but looks like that they should all be fixed with 'Z' model.
From the dev board schematic (
) I have disconnected jumper SB177 not to reset ETH controller after STM restarts. If I reset manually my ETH controller from the same jumper so that green LED stays off then I can do whatever with my STM (reprogram,...) then ethernet remains functional.To me it looks like the same issue as here which should be fixed now.
Currently, whatever I develop with my ethernet based nucleos I hit all the time with same issue. Any ideas?
#nucleo-f746 #ethernet #rmii #nucleo-f767zi