Question
STM32CubeF0 compilation using arm-none-eabi-gcc and Makefile.
Posted on October 28, 2014 at 09:39
I'm trying to get a STM32Cube project compiled using arm-none-eabi-gcc and a Makefile. I have specified:
CFLAGS = -mthumb\
-march=armv6-m\
-mlittle-endian\
-mcpu=cortex-m0\
-ffunction-sections\
-fdata-sections\
-MMD\
-std=c99\
-Wall\
-g\
-D$(PART)\
-c
and:
LDFLAGS = -Wl,--gc-sections\
-Wl,-T$(LDFILE)\
-Wl,-v
The FW builds without problems.but when I boot the MCU i get stuck in Hard Fault. Stack trace is:
#0 HardFault_Handler () at ./Src/main.c:156
#1 <
signal
handler called>
#2 0x0800221c in ____libc_init_array_from_thumb ()
#3 0x080021be in LoopFillZerobss () at Src/startup_stm32f030x8.s:103
#4 0x080021be in LoopFillZerobss () at Src/startup_stm32f030x8.s:103
Backtrace stopped: previous frame identical to this frame (corrupt stack?)
and I go straight to Hard Fault when stepping to bl __libc_init_array in the startup file.
/* Zero fill the bss segment. */
FillZerobss:
movs r3, #0
str r3, [r2]
adds r2, r2, #4
LoopFillZerobss:
ldr r3, = _ebss
cmp r2, r3
bcc FillZerobss
/* Call the clock system intitialization function.*/
bl SystemInit
/* Call static constructors */
bl __libc_init_array
/* Call the application's entry point.*/
bl main
Any ideas what could be wrong?
My arm-none-eabi-gcc version is 4.8.4 20140725 (release)
[edit] The disassembly of the calls
08002218 <
____libc_init_array_from_thumb
>:
8002218: 4778 bx pc
800221a: 46c0 nop ; (mov r8, r8)
800221c: eafff812 b 800026c <
__libc_init_array
>
0800026c <
__libc_init_array
>:
800026c: e92d4070 push {r4, r5, r6, lr}
8000270: e59f506c ldr r5, [pc, #108] ; 80002e4 <
__libc_init_array
+0x78>
8000274: e59f606c ldr r6, [pc, #108] ; 80002e8 <
__libc_init_array
+0x7c>
8000278: e0656006 rsb r6, r5, r6
800027c: e1b06146 asrs r6, r6, #2
8000280: 12455004 subne r5, r5, #4
8000284: 13a04000 movne r4, #0
8000288: 0a000005 beq 80002a4 <
__libc_init_array
+0x38>
800028c: e2844001 add r4, r4, #1
8000290: e5b53004 ldr r3, [r5, #4]!
8000294: e1a0e00f mov lr, pc
8000298: e12fff13 bx r3
800029c: e1560004 cmp r6, r4
80002a0: 1afffff9 bne 800028c <
__libc_init_array
+0x20>
80002a4: e59f5040 ldr r5, [pc, #64] ; 80002ec <
__libc_init_array
+0x80>
80002a8: e59f6040 ldr r6, [pc, #64] ; 80002f0 <
__libc_init_array
+0x84>
80002ac: e0656006 rsb r6, r5, r6
80002b0: eb0007ca bl 80021e0 <
_init
>
80002b4: e1b06146 asrs r6, r6, #2
80002b8: 12455004 subne r5, r5, #4
80002bc: 13a04000 movne r4, #0
80002c0: 0a000005 beq 80002dc <
__libc_init_array
+0x70>
80002c4: e2844001 add r4, r4, #1
80002c8: e5b53004 ldr r3, [r5, #4]!
80002cc: e1a0e00f mov lr, pc
80002d0: e12fff13 bx r3
80002d4: e1560004 cmp r6, r4
80002d8: 1afffff9 bne 80002c4 <
__libc_init_array
+0x58>
80002dc: e8bd4070 pop {r4, r5, r6, lr}
80002e0: e12fff1e bx lr
80002e4: 08002258 .word 0x08002258
80002e8: 08002258 .word 0x08002258
80002ec: 08002258 .word 0x08002258
80002f0: 08002260 .word 0x08002260
[edit 2] The register values from gdb:
(gdb) info reg
r0 0x20000000 536870912
r1 0x1 1
r2 0x0 0
r3 0x40021000 1073876992
r4 0xffffffff -1
r5 0xffffffff -1
r6 0xffffffff -1
r7 0x20001fd0 536879056
r8 0xffffffff -1
r9 0xffffffff -1
r10 0xffffffff -1
r11 0xffffffff -1
r12 0xffffffff -1
sp 0x20001fd0 0x20001fd0
lr 0xfffffff9 -7
pc 0x800067c 0x800067c <
HardFault_Handler
+4>
xPSR 0x61000003 1627389955
#gcc-arm-stm32-cortex-m-cubef0