Question
STM32Cube + F4-Discovery + FatFS
Posted on May 20, 2014 at 18:44
I'm trying to test out and utilize the STM32Cube configuration / code generation system to help get things on a new project started. The project is using an SD card, to which I want FatFS access internally. Ideally, I also want to get a dual-access system where the SD card is also mounted as a mass storage device over USB. I'll save that for later, though.
To try this out, I started with the STM32F4-Discovery board and the -BB base board with SD Card connector. I started with the base STM32Cube configuration using the new project dialog, then added the SDIO interface (disabling the conflicting interfaces), and FatFS. I left the default settings on there (no DMA or other interrupts). It did not work first time. I used the test function from the FatFS_USBDisk example application from the STM32Cube_FW_F4_V1.1.0 folders, MSC_Application(), just modified to use the FatFS SD Driver's path (SD_Path) from the generated code. I put a single call to this in the USER CODE 3 section in main() with a while(1); after it to catch everything. The default settings for FatFS, though are to use the _DMA functions for transfer, even if you have DMA disabled. And, if they have DMA enabled, they don't function correctly. 1) Here's how I got it working without DMA: I modified the calls in SD_read() within sd_diskio.c from BSP_SD_[Read/Write]Blocks_DMA() toBSP_SD_[Read/Write]Blocks(). Literally, just remove the ''_DMA''. Then, the FatFS system was failing to create files, etc. Tracking this down, I found the heap insufficient by default (0x0200). Raising this to 0x0300 fixed the problem. I would recommend making this higher, though. Both of these problems need to be fixed in the code generation tools: It shouldn't use the _DMA functions when DMA is disabled / not configured. The non-DMA functions are even completely written and available. Also, and the heap size should increase if using FatFS. 2) Now, how to get it working with DMA? First problem I've run into is that the DMA and SDIO interrupts were not configured, so it hung on the while loop in HAL_SD_CheckReadOperation():while ((tmp1 == 0) && (tmp2 == 0) && (tmp3 == SD_OK) && (timeout > 0))
{
tmp1 = hsd->DmaTransferCplt;
tmp2 = hsd->SdTransferCplt;
tmp3 = (HAL_SD_ErrorTypedef)hsd->SdTransferErr;
timeout--;
}
This made me realize that the DMA / SDIO interrupts weren't enabled, nor the DMA configured. So, I enabled them, regenerated the code, and now it hangs on this while loop in the same function:
/* Wait until the Rx transfer is no longer active */
while((__HAL_SD_SDIO_GET_FLAG(hsd, SDIO_FLAG_RXACT)) && (timeout > 0))
{
timeout--;
}
This is where I'm stuck. In researching further, looking at [DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/SDIO%20and%20SD%20fat%20access%20example&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=8757]Clive's FATFS-DBG example, it looks like it's re-configuring the DMA each transfer, which makes sense - using the same stream for each direction. However, I think this has something to do with the fact that with the code generation, it configures it once in MX_DMA_Init() and then links the DMA handle to two different ''handles''. This would imply that it would be reconfiguring the DMA as appropriate. However, within the HAL_SD_[Read/Write]Blocks_DMA() functions, the references tohsd->hdma[rx/tx] don't seem to ever reconfigure the *.Init structure, nor reinitialize the DMA like Clive's SD_LowLevel_DMA_[Rx/Tx]Config() functions do.
I think this needs to be fixed in the STM32Cube generator as well. I will proceed with trying to fix it, but I think that the Cube initiative was to prevent you having to edit the generated code.
This was to serve as both a PSA / information about getting it to worth without DMA and also a request for other thoughts about what might be wrong getting it to work with DMA.
Comments / thoughts welcome!
#stm32-fat-fatfs-sdio-dma