Question
Problem in Simultaneous Record and Play
Posted on September 11, 2015 at 18:30
Hi,
I'm trying to write an application to do simultaneous record and play on the STM32F4Discovery board. (16 KHz, 2 Channel, 16-bits). The audio quality on the speaker is not good in this case. Thereafter, I tried to do this sequentially instead of simultaneously. I first record into a 40960 bytes buffer and then play from that buffer. The sequence is:BSP_AUDIO_IN_Init()BSP_AUDIO_IN_Record()// Record SamplesBSP_AUDIO_IN_Stop()BSP_AUDIO_OUT_Init()BSP_AUDIO_OUT_Play()// Play the same bufferBSP_AUDIO_OUT_Stop() This sequence runs correctly for the first time and I'm able to hear the recorded audio correctly. But when I run this in a loop for the second time, the audio is highly distorted. I can barely make out what was spoken during recording. Could you please advise on anything that I might be doing wrong.thanks,Ngupta #stm32f4discovery-audio