Skip to main content
Ekaya.1
Visitor II
September 7, 2020
Question

printing parent id of folders

  • September 7, 2020
  • 0 replies
  • 933 views

Hi Community, I am working on a project which has Sd card with spi and using FATFS library.I want to store id ,parent id and short filename of all directories and subdirectories not files

0693W000003QyQNQA0.png

for example for this diagram my output will like :

id /name /parent id

1 / / /1

2 / bin /1

3 / usr /1

4 / local /3

5 / bin /3

6 / ucb /3

7 / home/ 1

8 / mkl /7

9 / mystuff /8

10 /stuff /9

11 /private/ 8

12 /hun /7

13 /hisstuff /12

14 /publick /12

15 /stuff /14

16 /other /7

i have researched the library and find this scanning function I can print all directory and subdirectories with id but no luck with parent ids any suggestion would be good for me

uint8_t id;

FRESULT scan_files (

char* path /* Start node to be scanned (***also used as work area***) */

)

{

FRESULT res;

DIR dir;

UINT i;

static FILINFO fno;

res = f_opendir(&dir, path); /* Open the directory */

if (res == FR_OK) {

for (;;) {

res = f_readdir(&dir, &fno); /* Read a directory item */

if (res != FR_OK || fno.fname[0] == 0) break; /* Break on error or end of dir */

if (fno.fattrib & AM_DIR) { /* It is a directory */

id++;

printf("%d %s",id,fno.altname);

i = strlen(path);

sprintf(&path[i], "/%s", fno.fname);

res = scan_files(path); /* Enter the directory */

if (res != FR_OK) break;

path[i] = 0;

}

}

f_closedir(&dir);

}

return res;

}

int main (void)

{

FATFS fs;

FRESULT res;

char buff[256];

res = f_mount(&fs, "", 1);

if (res == FR_OK) {

strcpy(buff, "/");

res = scan_files(buff);

}

return res;

}

This topic has been closed for replies.