Question
Pb with FreeRTOS and USB
Posted on January 05, 2012 at 13:26
Hello,
We are working on the STM3220-G Evaluation Board. We are using IAR compiler [V6.2] and running a test application with FreeRTOS [7.0.2] and the STM32_F105-07_F2xx_USB-Host-Device_Lib_V2.0.0 The USB is used as Virtual Com Port. The USB alone works correctly. The FreRTOS alone works correctly (with only one task). But when I put USB with FreeRTOS, I have systematically a crash on the IAR environnement (don't answer), I must close the environnment Have someone already have this kind of problem, please? Regards #usb #freertos #freertos #virtual-comm-port