Question
Leave DFU mode error
Posted on September 22, 2011 at 10:57
Hi all,
I am using DfuSe demo (v3.0.0) to communicate with the board STM3220G-eval. I am willing to test, understand and confirm the leave DFU sequence. So I press the button ''Leave DFU Mode'' on the DfuSe and i can see the process happening in the progress bar upto 49% completion, but then i received an ''unexpected error'' and cant leave the DFU mode. There are no issues with communication otherwise. I am able to load the binary into the flash and verify it successfully. The problem seems to occurring consistently at 49% completion. I also tested on different computers but on all computers i receive the same ''unexpected error'' at 49%. Have anybody seen this kind of behavior earlier? My goal is simply to leave the DFU mode using DfuSe utility. Can somebody please guide me to achieve my goal? Thanks #dfuse #leave-dfu-mode-error