Question
glitch-free initialization of GPIO-pins with HAL-LL possible?
I do LL_GPIO_SetOutputPin() before LL_GPIO_Init() so the ODR-Register is preloaded and the pin goes directly from Hi-Z to Highlevel. However, in LL_GPIO_Init() there is a call to LL_GPIO_SetPinPull() wich sets the ODR to an unwanted value. This call should only be done for Input-pins (in my opinion). I am using the STM32CubeMX-generated code (STM32Cube FW_F1 V1.8.0). The problematic behavior is in stm32f1xx_ll_gpio.c#196