Skip to main content
kajtek610
Associate II
December 14, 2018
Question

Ethernet stopped working after migrating to STM32F457IG MCU from STM3240G-EVAL Board

  • December 14, 2018
  • 0 replies
  • 574 views

Hi!

I have a working ethernet code on my STM3240G-EVAL Board with STM32F457IG MCU. By working i mean MCU responds my ping requests. I'm using FreeRTOS and of course LwIP. And now i want migrate to my own PCB with STM32F407ZG6 MCU. When I connect a DP83848 module with 15 cm wires (that's might be a problem) MCU doesn't respond. I can see frames on RXx pins and can not see any on TXx pins. All I've done by now in my software is remap GPIO Pins. I choose those ethernet pinout:

     PA0-WKUP   ------> ETH_CRS

     PA1   ------> ETH_RX_CLK

     PA2   ------> ETH_MDIO

     PA3   ------> ETH_COL

     PA7   ------> ETH_RX_DV

     PB0   ------> ETH_RXD2

     PB1   ------> ETH_RXD3

     //PB5  ------> PPS_OUT

     PB8   ------> ETH_TXD3

     PB10  ------> ETH_RX_ER

     PB11   ------> ETH_TX_EN

     PB12   ------> ETH_TXD0

     PB13   ------> ETH_TXD1

     PC1   ------> ETH_MDC

     PC2   ------> ETH_TXD2

     PC3   ------> ETH_TX_CLK

     PC4   ------> ETH_RXD0

     PC5   ------> ETH_RXD1

And actually that's all i've changed in my code, ETH and DMA settings are the same. Oh and one more thing, because i don't use a ,,Link status interrupt'', i check Link Status in DP83848 register now and then in FreeRTOS task, it seems all right in debugger. And now my question: is there anything else i should changed in firmwere when migrating between this two MCU which i think are almost the same (core, buses, peripherials etc.). Or maybe it has to be a hardware issue.

Thanks a lot in advance

This topic has been closed for replies.