Skip to main content
nSTAC.1
Associate
May 25, 2020
Question

[Bug] Channel 8 (and over) of DMA stream lead to code generation error on UART

  • May 25, 2020
  • 1 reply
  • 533 views

Hello,

I use:

CubeIDE 1.3.0

STM32Cube_FW_F4_1.25.0

STM32F413CHU

I want to use DMA on UART5 on this uC but generated code (from CubeIDE) does not compile.

Channel used by this UART is DMA1->Stream7->Channel8

I use LL, not HAL for UART.

Into MX_UART5_Init function (Core/Src/usart.c), called in main, there is this following line:

LL_DMA_SetChannelSelection(DMA1, LL_DMA_STREAM_7, DMA_CHANNEL_8);

Unfortunately,DMA_CHANNEL_8 is not defined.

Actually, DMA_CHANNEL_x are not defined. However LL_DMA_CHANNEL_1 to LL_DMA_CHANNEL_7 are defined.

I added LL_DMA_CHANNEL_8 (into Drivers/STM32F4xx_HAL_Driver/STM32F4xx_ll_dma.h):

#define LL_DMA_CHANNEL_8 DMA_SxCR_CHSEL_3

I replaced DMA_CHANNEL_8 to LL_DMA_CHANNEL_8 and my code is compiling.

My code generation produces an error.

I asked for help on ST Community platform:

https://community.st.com/s/question/0D53W000007ZZPxSAO/channel-8-and-over-of-dma-stream-lead-to-code-generation-error-on-uart

TDK member suggested an omission. "They [DMA channels from 8] are defined within stm32f4xx_hal_dma.h but not within stm32f4xx_ll_dma.h"

I hope this post will help you.

Thanks for your help.

This topic has been closed for replies.

1 reply

Imen GH
ST Employee
June 3, 2020

Hello @nSTAC.1​ ,

I take your feedback into consideration and I will raise this internally.

Thank you

Regards