Skip to main content
DeveloperMan
Associate III
August 7, 2020
Question

Bootloader-RS485

  • August 7, 2020
  • 3 replies
  • 1891 views

Hello there,

I want to load the application code with the bootloader over the RS-485 line using stm32f103 in my project. I did this over the RS-232 line. However, I could not achieve this with the RS-485 line.

This topic has been closed for replies.

3 replies

Tesla DeLorean
Guru
August 7, 2020

I wouldn't expect the ROM based system loader to be able to support this mode of connection.

You'll need to code your own loader with awareness of your hardware design.

Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
DeveloperMan
Associate III
August 10, 2020

I can boot the software with Real-Term via the CPU's usart1 pins (Tx-Rx). However, there is an RS-485 integrated in my hardware and there is a conversion with the A-B line. In order to turn this hardware into software, I need to configure it over the enable pin.

TDK
Super User
August 7, 2020

The STM32F1 doesn't have native support for RS-232 or RS-485. You'll need a transceiver chip to convert it to a single ended signal and hook it up to one of the UART ports supported by the bootloader.

"If you feel a post has answered your question, please click ""Accept as Solution""."
DeveloperMan
Associate III
August 10, 2020

What exactly do you mean by the transceiver chip?

prain
Visitor II
August 7, 2020

You can use a custom Bootloader to achieve this.

The default ST Bootloader work in full duplex mode​, so you can use RS422 instead.

DeveloperMan
Associate III
August 10, 2020

I can boot the software with Real-Term via the CPU's usart1 pins (Tx-Rx). However, there is an RS-485 integrated in my hardware and there is a conversion with the A-B line. In order to turn this hardware into software, I need to configure it over the enable pin.