Skip to main content
Ala
Senior
April 26, 2020
Question

Audio Codec

  • April 26, 2020
  • 0 replies
  • 883 views

Hi

I have a STM32F407 Discovery board which I wish to use its Audio codec demonstrated by CS43L22 ic. here is my code(I used Cube)

 */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include "stm32f4xx_hal.h"
#include "MY_CS43L22.h"
#include <math.h>
/* USER CODE BEGIN Includes */
 
/* USER CODE END Includes */
 
/* Private variables ---------------------------------------------------------*/
DAC_HandleTypeDef hdac;
 
I2C_HandleTypeDef hi2c1;
 
I2S_HandleTypeDef hi2s3;
DMA_HandleTypeDef hdma_spi3_tx;
 
TIM_HandleTypeDef htim2;
 
/* USER CODE BEGIN PV */
/* Private variables ---------------------------------------------------------*/
 
/* USER CODE END PV */
 
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
void Error_Handler(void);
static void MX_GPIO_Init(void);
static void MX_DMA_Init(void);
static void MX_DAC_Init(void);
static void MX_I2C1_Init(void);
static void MX_I2S3_Init(void);
static void MX_TIM2_Init(void);
 
/* USER CODE BEGIN PFP */
/* Private function prototypes -----------------------------------------------*/
 
/* USER CODE END PFP */
 
/* USER CODE BEGIN 0 */
float mySinVal;
uint16_t i_t;
uint16_t sample_N;
float sample_dt;
uint32_t myDacVal;
#define PI 3.14159f
#define F_SAMPLE 50000.0f //sample rate
#define F_OUT 1000.0f //output frequency
uint16_t I2S_dummy[4];
/* USER CODE END 0 */
 
int main(void)
{
sample_dt =F_OUT/F_SAMPLE;
sample_N =F_SAMPLE/F_OUT;	
 /* USER CODE BEGIN 1 */
 
 /* USER CODE END 1 */
 
 /* MCU Configuration----------------------------------------------------------*/
 
 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();
 
 /* Configure the system clock */
 SystemClock_Config();
 
 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_DMA_Init();
 MX_DAC_Init();
 MX_I2C1_Init();
 MX_I2S3_Init();
 MX_TIM2_Init();
 
 /* USER CODE BEGIN 2 */
CS43_Init(hi2c1,MODE_ANALOG);
CS43_SetVolume(100);
CS43_Enable_RightLeft(CS43_RIGHT_LEFT);
CS43_Start();
 
HAL_I2S_Transmit_DMA(&hi2s3,(uint16_t *)I2S_dummy,4);
 /* USER CODE END 2 */
HAL_DAC_Start(&hdac,DAC_CHANNEL_1);
HAL_TIM_Base_Start_IT(&htim2);
 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */
 
 /* USER CODE BEGIN 3 */
 
 }
 /* USER CODE END 3 */
 
}
 
/** System Clock Configuration
*/
void SystemClock_Config(void)
{
 
 RCC_OscInitTypeDef RCC_OscInitStruct;
 RCC_ClkInitTypeDef RCC_ClkInitStruct;
 RCC_PeriphCLKInitTypeDef PeriphClkInitStruct;
 
 /**Configure the main internal regulator output voltage 
 */
 __HAL_RCC_PWR_CLK_ENABLE();
 
 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
 
 /**Initializes the CPU, AHB and APB busses clocks 
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
 RCC_OscInitStruct.HSEState = RCC_HSE_ON;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
 RCC_OscInitStruct.PLL.PLLM = 4;
 RCC_OscInitStruct.PLL.PLLN = 168;
 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
 RCC_OscInitStruct.PLL.PLLQ = 4;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }
 
 /**Initializes the CPU, AHB and APB busses clocks 
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;
 
 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5) != HAL_OK)
 {
 Error_Handler();
 }
 
 PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_I2S;
 PeriphClkInitStruct.PLLI2S.PLLI2SN = 50;
 PeriphClkInitStruct.PLLI2S.PLLI2SR = 2;
 if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
 {
 Error_Handler();
 }
 
 /**Configure the Systick interrupt time 
 */
 HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);
 
 /**Configure the Systick 
 */
 HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);
 
 /* SysTick_IRQn interrupt configuration */
 HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);
}
 
/* DAC init function */
static void MX_DAC_Init(void)
{
 
 DAC_ChannelConfTypeDef sConfig;
 
 /**DAC Initialization 
 */
 hdac.Instance = DAC;
 if (HAL_DAC_Init(&hdac) != HAL_OK)
 {
 Error_Handler();
 }
 
 /**DAC channel OUT1 config 
 */
 sConfig.DAC_Trigger = DAC_TRIGGER_NONE;
 sConfig.DAC_OutputBuffer = DAC_OUTPUTBUFFER_ENABLE;
 if (HAL_DAC_ConfigChannel(&hdac, &sConfig, DAC_CHANNEL_1) != HAL_OK)
 {
 Error_Handler();
 }
 
}
 
/* I2C1 init function */
static void MX_I2C1_Init(void)
{
 
 hi2c1.Instance = I2C1;
 hi2c1.Init.ClockSpeed = 100000;
 hi2c1.Init.DutyCycle = I2C_DUTYCYCLE_2;
 hi2c1.Init.OwnAddress1 = 0;
 hi2c1.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
 hi2c1.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
 hi2c1.Init.OwnAddress2 = 0;
 hi2c1.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
 hi2c1.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;
 if (HAL_I2C_Init(&hi2c1) != HAL_OK)
 {
 Error_Handler();
 }
 
}
 
/* I2S3 init function */
static void MX_I2S3_Init(void)
{
 
 hi2s3.Instance = SPI3;
 hi2s3.Init.Mode = I2S_MODE_MASTER_TX;
 hi2s3.Init.Standard = I2S_STANDARD_PHILIPS;
 hi2s3.Init.DataFormat = I2S_DATAFORMAT_16B;
 hi2s3.Init.MCLKOutput = I2S_MCLKOUTPUT_ENABLE;
 hi2s3.Init.AudioFreq = I2S_AUDIOFREQ_48K;
 hi2s3.Init.CPOL = I2S_CPOL_LOW;
 hi2s3.Init.ClockSource = I2S_CLOCK_PLL;
 hi2s3.Init.FullDuplexMode = I2S_FULLDUPLEXMODE_DISABLE;
 if (HAL_I2S_Init(&hi2s3) != HAL_OK)
 {
 Error_Handler();
 }
 
}
 
/* TIM2 init function */
static void MX_TIM2_Init(void)
{
 
 TIM_ClockConfigTypeDef sClockSourceConfig;
 TIM_MasterConfigTypeDef sMasterConfig;
 
 htim2.Instance = TIM2;
 htim2.Init.Prescaler = 84-1;
 htim2.Init.CounterMode = TIM_COUNTERMODE_UP;
 htim2.Init.Period = 20-1;
 htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
 if (HAL_TIM_Base_Init(&htim2) != HAL_OK)
 {
 Error_Handler();
 }
 
 sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
 if (HAL_TIM_ConfigClockSource(&htim2, &sClockSourceConfig) != HAL_OK)
 {
 Error_Handler();
 }
 
 sMasterConfig.MasterOutputTrigger = TIM_TRGO_UPDATE;
 sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
 if (HAL_TIMEx_MasterConfigSynchronization(&htim2, &sMasterConfig) != HAL_OK)
 {
 Error_Handler();
 }
 
}
 
/** 
 * Enable DMA controller clock
 */
static void MX_DMA_Init(void) 
{
 /* DMA controller clock enable */
 __HAL_RCC_DMA1_CLK_ENABLE();
 
 /* DMA interrupt init */
 /* DMA1_Stream5_IRQn interrupt configuration */
 HAL_NVIC_SetPriority(DMA1_Stream5_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(DMA1_Stream5_IRQn);
 
}
 
/** Configure pins as 
 * Analog 
 * Input 
 * Output
 * EVENT_OUT
 * EXTI
*/
static void MX_GPIO_Init(void)
{
 
 GPIO_InitTypeDef GPIO_InitStruct;
 
 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOH_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();
 __HAL_RCC_GPIOD_CLK_ENABLE();
 __HAL_RCC_GPIOC_CLK_ENABLE();
 __HAL_RCC_GPIOB_CLK_ENABLE();
 
 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12|GPIO_PIN_13|GPIO_PIN_14|GPIO_PIN_15 
 |GPIO_PIN_4, GPIO_PIN_RESET);
 
 /*Configure GPIO pins : PD12 PD13 PD14 PD15 
 PD4 */
 GPIO_InitStruct.Pin = GPIO_PIN_12|GPIO_PIN_13|GPIO_PIN_14|GPIO_PIN_15 
 |GPIO_PIN_4;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);
 
}
 
/* USER CODE BEGIN 4 */
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
{
 /* Prevent unused argument(s) compilation warning */
 UNUSED(htim);
 /* NOTE : This function Should not be modified, when the callback is needed,
 the __HAL_TIM_PeriodElapsedCallback could be implemented in the user file
 */
	if(htim->Instance==TIM2){
	mySinVal=sinf(i_t*2*PI*sample_dt);
	myDacVal=(mySinVal+1)*127;
	HAL_DAC_SetValue(&hdac,DAC_CHANNEL_1,DAC_ALIGN_8B_R,myDacVal);
	i_t++;
	if(i_t>=sample_N) i_t=0;	
	}
}
/* USER CODE END 4 */
 
/**
 * @brief This function is executed in case of error occurrence.
 * @param None
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler */
 /* User can add his own implementation to report the HAL error return state */
 while(1) 
 {
 }
 /* USER CODE END Error_Handler */ 
}
 
#ifdef USE_FULL_ASSERT
 
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * @param file: pointer to the source file name
 * @param line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t* file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
 
}
 
#endif
 
/**
 * @}
 */ 
 
/**
 * @}
*/ 
 
/************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/

a while ago, I plugged the USB in and loaded the program without any errors. but now when I'm trying to do the same, the red LED on the top(LED1) starts to blink and the USB is not recognized... help!

This topic has been closed for replies.