How to deal with I2C Communication for the slave x-nucleo-nfc07a1 in which ST25DV64KC incorporated and is interfaced with STM32WB55RG?
- May 23, 2023
- 2 replies
- 3195 views
Hi Sir/Madam,
I am working with I2C in x-nucleo-nfc07a1 where ST25DV IC incorporated interfaced with Nucleo-WB55 board, what is the slave address(device address) for this?
I am firmware engineer, I have I2C Scanning program where
Previously, I work with Temp sensor, the scanning code gives me slave address as 0x4a,
I also work the following,
Heart rate sensor in which it is 0x57
PN532 NFC reader in which it shows 0x24
And right now I work with X-Nucleo-NFC07A1 in which ST25DV64KC is incorporated, here the scanning code shows none. I want to know, why it is not? and how to deal with i2c communication to store data in EEPROM? HAL_I2c functions deals with 5 parameters, DevAddr, TargetAddr, Data Buffer, No.of.Bytes req, delay, out of which DevAddr what we can use?
In the datasheet of ST25DV64KC, Table 89 Device select code and Table 91 I2C CFG are confusing with the bit assignment. I also attach the respective datasheet for your reference.
Best Regards,
Bhuvaneswaran T