STM32 MCUs products

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

UCPD SINK Application NUCLEO-u575ZI-Q

I'm trying to run a simple UCPD SINK application on the NUCLEO-U575ZI-Q.I attempted to follow the example provided here: https://wiki.stmicroelectronics.cn/stm32mcu/wiki/STM32StepByStep:Getting_started_with_USB-Power_Delivery_Sink#-5BOPTIONAL-5D_Conf...

acipriano_1-1713372587747.png acipriano_2-1713372661433.png

Resolved! STM32F4 Series a Question About I2S

Hi, I am trying to do an application where I am using 2 PDM output digital MEMS microphones to get a stereo sound from them and then play it. My question is when I select I2S as Full-Duplex Master for STM32F407VG it only has 1 SD pin. Should connect ...

mdmrl00 by Associate II
  • 38 Views
  • 3 replies
  • 1 kudos

STM32F4 SPI high level 5V

Sorry, I have another question to ask everyone. I'm currently using the Nucleo F429ZI with SPI interface to receive 12-bit encoded data from another ADC. The Vdrive of that ADC can provide 3.3V or 5V for driving. However, the high level of the STM32F...

Scarlet_0-1713766357977.png
Scarlet by Associate II
  • 543 Views
  • 29 replies
  • 14 kudos

STM32F405 ULPI USB3343

Hello Guys,I am new to STM and USB HS but have some experience with PICs and other AVRs. I've designed my own custom board (for a keyboard). So after I generated the USB HID code with STM32cube IDE, I successfully downloaded it to the STM, however, n...

maubla by Visitor
  • 34 Views
  • 2 replies
  • 0 kudos

Delay in SPI Transfer with STM32H7

Dear ForumIm using STM32 H755 ZI in the starter kit. I set the Timer 4 for generate a Interrupt each 1ms.At begin of INT:     -I toggle a PIN,      -and, send a SPI data (8 byte or 16..not important)What I noted is a delay of almost 10uS beetwen pin ...

Roibert by Associate
  • 94 Views
  • 4 replies
  • 0 kudos

NOR Flash(external memory )- Status error

Hi all, I'm working on the NOR Flash via OSPI(using as QSPI) with the STM32U585 board. implementing this via filex and levelx, i have done all the configuration referring to the example provided by ST with the minor changes. I'm getting error in the ...

meghasb by Senior
  • 67 Views
  • 1 replies
  • 1 kudos