Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STEVAL-KITXCB SD pin question

In STEVAL-KITXCB for controlling SD/OD pin of L6491 using such method. PWM_en connected to MCU pin. I want use same principle in my design. Can anybody describe how program this.Is such hw connection support both function for enable PWM and for contr...

Без імені.png
Kuzma30 by Associate II
  • 40 Views
  • 3 replies
  • 0 kudos

eDesignSuite Transformer

Hello I tried to design a 3-output AC-DC converter using the eDesignSuite. But the software only provides the turns ratio for the transformer and no core suggestions or what so ever was shown.I don't get the idea behind the eDesignSuite software that...

info23 by Associate
  • 42 Views
  • 0 replies
  • 0 kudos

Resolved! How to set STUSB4710 PDO profiles

Hi, I am designing a 25W power supply for the raspberry pi 5 for my battery powered project. The buck regulator I am using has a fixed 5V output and I want to use the STUSB4710 to offer 5V 5A to the Pi. How can I program the registers to do so via I2...

CMaker by Associate
  • 200 Views
  • 1 replies
  • 0 kudos

Three phase capacitive power supply transformerless

I need to use in our application three phase power supply any of the two phase present power supply should work or with respect neutral also work if any of one phase present.  required for voltage monitoring three phase or sequence detector. any refe...

Glodhi by Associate II
  • 40 Views
  • 1 replies
  • 1 kudos

VN7003: Short circuit protection failure

Dear ST Technical Support,I would like to inquire about the short-circuit protection behavior of the VN7003ALH high-side switch.Application: Board with 6× VN7003ALH outputs.Configuration: 24V supply from 200Ah lead-acid battery. Output wiring: 1.5m o...

0-02-05-3337e733268341aeeec74b6495bb0ac832b8fbc8370f2b23150e5f58a236b94e_4aeeb4d35658a96.jpg 0-02-05-9c1fff7c2a0268fa4807d0197e6ff417b977b7ea487547fcc2036345f1ecff2a_a7140ec006b7b8a7.jpg Minloud_0-1770234130646.png
Minloud by Associate
  • 50 Views
  • 0 replies
  • 0 kudos

VNQ9080AJ Flyback diodes for inductive loads

Hi,I'm designing a custom PCB and I'll be using a VNQ9080AJ to drive 4 inductive loads (hydraulic valve spools).Is the protection diode in the datasheet sufficient for that application?The device will drive up to 28 VDC ~3.5 to 5 amps inductive loads...

emachabeeinnotag_0-1769613302763.png