STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USBPD EPR Sink

Following this thread Solved: USBPD EPR Source - STMicroelectronics Community Do you have a similar guide on how to do EPR as a Sink?

xGloooM by Associate II
  • 57 Views
  • 2 replies
  • 0 kudos

Official STM32 Bootloader

Hi, I need to update the firmware of my MCU from the UART. I mean without physically touching the BOOT pin, but only via serial commands (classic FW update of a product).I'm not an expert, but I tried searching on the internet and I saw that for thes...

FMass.1 by Associate III
  • 53381 Views
  • 6 replies
  • 6 kudos

SysTick Callback not being generated?

Hi,I am using a STM32C031G6U6 and I would appreciate some clarification regarding HAL timebase and SysTick timebase selection.I want to use SysTick as a 1ms interrupt so in CubeMX I selected SysTick as timebase (see screenshot): None of the other tim...

Ricko_0-1770359921026.png Ricko_1-1770360000600.png Ricko_1-1770361629621.png Ricko_0-1770361610071.png
Ricko by Senior III
  • 61 Views
  • 4 replies
  • 0 kudos