STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 3672 Views
  • 0 replies
  • 2 kudos

Using ADCCTRL to read an external voltage

Starting with the BLE_Heartrate example, I want to measure a voltage on PA8 of STM32WBA65. The BLE_Heartrate project already has the option of using ADCCTRL to read the internal temperature so as to calibrate the BLE power.I have added PA8 as ADC_Cha...

SLevi.1 by Senior
  • 114 Views
  • 2 replies
  • 0 kudos

STM32WB55 BLE Beacon Advertisement Update

Hi all,I’m working on an STM32WB55 and trying to run two advertisements “in parallel”:a connectable advertisement (for normal connections / data)a non-connectable advertisement using Additional BeaconI can see both advertisements from an Android devi...

DenysK by Associate III
  • 172 Views
  • 3 replies
  • 0 kudos

STM32WB05TZ fails MX_RTC_Init()

I have a problem with the RTC initialization on the STM32WB05TZF6TR (BGA package).  When the board is powered on, the MX_RTC_Init() function calls HAL_RTC_Init(), which returns with HAL_ERROR status.I traced the problem to the stm32wb0x_hal_rtc.c fil...

DG_NC by Associate
  • 79 Views
  • 2 replies
  • 0 kudos

Resolved! STM32WL33x default SWD pins

Hello all :)I am designing a board using the STM32WL33CCV6TR, and want to program/debug using the SWD interface. However, there are multiple pins the SWDIO and SWCLK can be mapped to using alternate functions. Usually with STM products, I have seen a...

angus123 by Associate III
  • 699 Views
  • 4 replies
  • 3 kudos

Project SBSFU_2_Slots_DualCore for Nucleo-WL55JC1

Hi,I'm using a Nucleo stm32WL55JC1 board, and i'm trying to run the SBSFU_2_Slots_DualCore example. Used the example selector to start the project. When I tried to compile any of the sub projects they all fail and i have a lot of warnings for include...

Untitled.png
Alfonzo by Associate II
  • 173 Views
  • 4 replies
  • 2 kudos

Resolved! P-NUCLEO WB55 - Arduino setup and basic examples

Hi,I am trying to make a basic Enhanced Advertising low power application using Arduino IDE.I use a standard P-NUCLEO WB55.I need Arduino IDE because this application is intended to be open for modifications.The current STM Documentation (https://wik...

fbd38 by Associate
  • 109 Views
  • 3 replies
  • 3 kudos