Where the configuration is stored in STVP
I would like to know where the configuration set in STVP is stored.I'd like to set the configuration automatically, but I don't know where the default storage address is.
I would like to know where the configuration set in STVP is stored.I'd like to set the configuration automatically, but I don't know where the default storage address is.
I download firmware in s19 format via STVP program.I would like to know how to check the checksum of firmware via STVP_Cmdline.How can I check it through the command?
Hello,I am using the STEVAL-IDB012V1 module, can you please tell me how I can test it? program it?
I have followed AN2959 and have a bootloader running on an STM8S Discovery board but I cannot make either the command line or GUI based STMFlashLoader programs upload a program - can anyone help?- The command line version always says `No response fro...
I am using the STM8S bootloader via a USB/FTDI. I can use Wireshark/USBpcap and catch the exchanges and I have a somewhat happy "export packets, parse with Python" method of looking at the exchange.But has anyone already written a proper Wireshark d...
AN2659, section 4.1.3 Vector table redirection, says that "The primary interrupt table contains a set of jumps to the user interrupt table" but the same code that accompanies this document does not seem to implement this - does this code just need to...
I have seen a number of questions about reading the stm8s mapfiles and I was also someone who struggled so the attached tool might be helpful (and do let me know of any errors!).The key elements are:- There are some elements that are stored in ROM ("...
I have a very simple main using UART1 and already my application is 7kB! The web implies that this is because I am getting a lot of UART1 and CLK code built and linked in that I am never using. One suggestion is to split the UART1 and CLK files int...
Getting stuck installing STM8CubeMX on Ubuntu 23.10.Downloaded from here: https://www.st.com/en/development-tools/stm8cubemx.html From the manual found here: https://www.st.com/resource/en/user_manual/um2125-stm8-configuration-tool-stmicroelectronics...
Hello all. I have an ISR inside which I want to disable and enable interrupts. Reference manual says : https://www.st.com/resource/en/reference_manual/rm0016-stm8s-series-and-stm8af-series-8bit-microcontrollers-stmicroelectronics.pdf Disabling the ...