LSM6DSO32X and clock sampling rate consistency
How consistent is the LSM6 sampling clock? I didn't see any details regarding clock variation at different temperatures, etc in the manual. However, I may have missed it.
How consistent is the LSM6 sampling clock? I didn't see any details regarding clock variation at different temperatures, etc in the manual. However, I may have missed it.
I am a bit confused about changing the Gyroscope Full-Scale range during operation (dynamically). Do I only need to change register CTRL2_G, or anything else too, to trigger a change to the Full-Scale range? What happens once I change the sensitivit...
HiI'm currently using your LPS22DFmodule to measure pressure and I saw in the datasheet that the temperature accuracy is ±1.5 °C (T = 0 to 80°C). My working range is between -15°C and 60°C. Could you please give me the accuracy of this sensor in the...
Hi I use a nucleo L432KC for a POC with an ASM330LHH. I use the internal FIFO of the ASM330 to store accelerator and gyroscope datas. I use an SPI to get datas periodically.During developpment, we used the 3.3V of the nucleo to supply the ASM330. We ...
Hi,We're using the lsm6dsv's SFLP algorithm to calculate IMU rotation. Recently however we noticed that the resulting rotation has big gaps at around the 180degree mark. We believe this is because of the half float precision, specifically because the...
Hello ST Community, I am currently working on a flight computer for a model rocket. It will be used together with a barometric pressure to estimate the altitude. It would be very nice if someone could review my schematic and point out any mistakes. ...
Hi all,I'm trying to use the LIS3DH to detect if the object is in a non-safe position, i.e. standing on a slope (tilted) or in the upside down position and generates an interrupt if it's one of these. Setup:Y-axis pointing downwards in the stable pos...
Hello,I have been battling with getting an LSM303AGR to pass the self test. The accelerometer is passing the self test and the values look reasonable (Z-axis ~1g), but the magnetometer will not pass. I have 2 STEVAL-MKI172V1 boards, both are showing ...
Is it necessary to enable Free Fall detection in order to detect orientation changes? What role does Free Fall (FF) play in this context? Additionally, is there a way to set a threshold force for detecting orientation changes, such as when the IMU is...
Hi Problems with a iio interface and using of buffer. Goal use the iio buffer interface for accel x y, z and temperture values. Include one Channel more for the temperature. static const struct iio_chan_spec st_accel_12bit_channels_temp[] = {S...