STM32 MPUs Embedded software

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Two ADC in dual REGULAR SIMULTENIOUS mode

I am trying to run both ADC in dual REGULAR SIMULTENIOUS mode (ADC1 as master and ADC2 as salve) ADC Converted Result shall be stored in an Array Buffer using DMA transfer (single channel only), ADC conversion trigger shall not be software based (we ...

Pooja321 by Associate II
  • 26 Views
  • 2 replies
  • 0 kudos

Problems with DCMI DMA callback registration. Environment: MCU: STM32MP157/M4; SW: STM32Cube FW_MP1 V1.6.0; Engineering Boot Mode

Hi all!Environment: I use MX to configure the DCMI Peripheral including DMA!MX generates MX_DMA_Init() and MX_DCMI_Init()After DCMI initialization in main with the above mentioned functions I use the functions HAL_DMA_RegisterCallback(&hdma_dcmi, HAL...

MLENG.1 by Associate
  • 525 Views
  • 1 replies
  • 1 kudos

confirm perspective switch tab

Hi , I am new to this boardI got this dialog box while starting the debug session as per start up guide.Board:STM32MP157D-DK1https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157x-DK2/Develop_on_Arm%C2%AE_Cortex%C2%AE-M4/Modify...

Screenshot from 2024-03-19 15-19-08.png Screenshot from 2024-03-19 15-29-06.png

Resolved! Linux kernel Build Fails

i am using ubuntu 22.04 ltsThe above mentioned photo  is what was the output when i follow Readfile. How to do.txt;i cannot able to figure out what was the issue.And because of this issue i am getting this issue isn't it?  (below attached)Now this er...

Screenshot from 2024-03-12 16-53-58.png Screenshot from 2024-03-12 16-08-48.png Screenshot from 2024-03-12 17-07-44.png

Resolved! XGboost model for STM32MP157D-DK1

Hello, I was wondering by using X-AI package. Will I be able to use the XGboost model converted to ONXX format in STM32 MP157 A7 core.  Or it only supports Neural Network models? I was browsing through the forum and found that ONXX runtime recipe is ...

meme002 by Associate II
  • 544 Views
  • 6 replies
  • 1 kudos