Skip to main content
Schuyler
Associate III
March 15, 2023
Solved

code to read and write NDEF on X-NUCLEO-NFC07A1

Can the following code be used to enable the phone to read and write NDEF messages?

I use X-NUCLEO-NFC07A1 and NUCLEO-L476RG

/* USER CODE BEGIN Header */
 
/**
 
 ******************************************************************************
 
 * @file : main.c
 
 * @brief : Main program body
 
 ******************************************************************************
 
 * @attention
 
 *
 
 * Copyright (c) 2021 STMicroelectronics.
 
 * All rights reserved.
 
 *
 
 * This software is licensed under terms that can be found in the LICENSE file
 
 * in the root directory of this software component.
 
 * If no LICENSE file comes with this software, it is provided AS-IS.
 
 *
 
 ******************************************************************************
 
 */
 
/* USER CODE END Header */
 
/* Includes ------------------------------------------------------------------*/
 
#include "main.h"
 
#include "app_nfc7.h"
 
#include "lib_NDEF.h"
 
/* Private includes ----------------------------------------------------------*/
 
/* USER CODE BEGIN Includes */
 
 
 
 
 
 
 
/* USER CODE END Includes */
 
 
 
/* Private typedef -----------------------------------------------------------*/
 
/* USER CODE BEGIN PTD */
 
 
 
/* USER CODE END PTD */
 
 
 
/* Private define ------------------------------------------------------------*/
 
/* USER CODE BEGIN PD */
 
/* USER CODE END PD */
 
 
 
/* Private macro -------------------------------------------------------------*/
 
/* USER CODE BEGIN PM */
 
 
 
/* USER CODE END PM */
 
 
 
/* Private variables ---------------------------------------------------------*/
 
 
 
/* USER CODE BEGIN PV */
 
 
 
/* USER CODE END PV */
 
 
 
/* Private function prototypes -----------------------------------------------*/
 
void SystemClock_Config(void);
 
static void MX_GPIO_Init(void);
 
/* USER CODE BEGIN PFP */
 
 
 
/* USER CODE END PFP */
 
 
 
/* Private user code ---------------------------------------------------------*/
 
/* USER CODE BEGIN 0 */
 
 
 
/* USER CODE END 0 */
 
 
 
/**
 
 * @brief The application entry point.
 
 * @retval int
 
 */
 
int main(void)
 
{
 
 /* USER CODE BEGIN 1 */
 
 uint8_t data[] = "Hello, world!";
 
 // 创建NDEF消�?�
 
 NDEF_WriteNDEF(strlen((char *)data), data);
 
 //读�?�NDEF消�?�
 
 NDEF_ReadNDEF(data);
 
 
 
 /* USER CODE END 1 */
 
 
 
 /* MCU Configuration--------------------------------------------------------*/
 
 
 
 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 
 HAL_Init();
 
 
 
 /* USER CODE BEGIN Init */
 
 
 
 /* USER CODE END Init */
 
 
 
 /* Configure the system clock */
 
 SystemClock_Config();
 
 
 
 /* USER CODE BEGIN SysInit */
 
 
 
 /* USER CODE END SysInit */
 
 
 
 /* Initialize all configured peripherals */
 
 MX_GPIO_Init();
 
 MX_NFC7_Init();
 
 /* USER CODE BEGIN 2 */
 
 
 
 /* USER CODE END 2 */
 
 
 
 /* Infinite loop */
 
 /* USER CODE BEGIN WHILE */
 
 while (1)
 
 {
 
 
 
 /* USER CODE END WHILE */
 
 
 
 MX_NFC7_Process();
 
 /* USER CODE BEGIN 3 */
 
 }
 
 /* USER CODE END 3 */
 
}
 
 
 
 
 
/**
 
 * @brief System Clock Configuration
 
 * @retval None
 
 */
 
void SystemClock_Config(void)
 
{
 
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
 
 
 
 /** Configure the main internal regulator output voltage
 
 */
 
 if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1) != HAL_OK)
 
 {
 
 Error_Handler();
 
 }
 
 /** Initializes the RCC Oscillators according to the specified parameters
 
 * in the RCC_OscInitTypeDef structure.
 
 */
 
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
 
 RCC_OscInitStruct.HSIState = RCC_HSI_ON;
 
 RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
 
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
 
 RCC_OscInitStruct.PLL.PLLM = 1;
 
 RCC_OscInitStruct.PLL.PLLN = 10;
 
 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV7;
 
 RCC_OscInitStruct.PLL.PLLQ = RCC_PLLQ_DIV2;
 
 RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV2;
 
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 
 {
 
 Error_Handler();
 
 }
 
 /** Initializes the CPU, AHB and APB buses clocks
 
 */
 
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
 
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
 
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
 
 
 
 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_4) != HAL_OK)
 
 {
 
 Error_Handler();
 
 }
 
}
 
 
 
/**
 
 * @brief GPIO Initialization Function
 
 * @param None
 
 * @retval None
 
 */
 
static void MX_GPIO_Init(void)
 
{
 
 GPIO_InitTypeDef GPIO_InitStruct = {0};
 
 
 
 /* GPIO Ports Clock Enable */
 
 __HAL_RCC_GPIOC_CLK_ENABLE();
 
 __HAL_RCC_GPIOH_CLK_ENABLE();
 
 __HAL_RCC_GPIOA_CLK_ENABLE();
 
 __HAL_RCC_GPIOB_CLK_ENABLE();
 
 
 
 /*Configure GPIO pin Output Level */
 
 HAL_GPIO_WritePin(GPIOA, LD2_Pin|GPIO_PIN_10, GPIO_PIN_RESET);
 
 
 
 /*Configure GPIO pin Output Level */
 
 HAL_GPIO_WritePin(GPIOB, GPIO_PIN_4|GPIO_PIN_5, GPIO_PIN_RESET);
 
 
 
 /*Configure GPIO pin : B1_Pin */
 
 GPIO_InitStruct.Pin = B1_Pin;
 
 GPIO_InitStruct.Mode = GPIO_MODE_IT_FALLING;
 
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 
 HAL_GPIO_Init(B1_GPIO_Port, &GPIO_InitStruct);
 
 
 
 /*Configure GPIO pins : USART_TX_Pin USART_RX_Pin */
 
 GPIO_InitStruct.Pin = USART_TX_Pin|USART_RX_Pin;
 
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
 
 GPIO_InitStruct.Alternate = GPIO_AF7_USART2;
 
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
 
 
 
 /*Configure GPIO pins : LD2_Pin PA10 */
 
 GPIO_InitStruct.Pin = LD2_Pin|GPIO_PIN_10;
 
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
 
 
 
 /*Configure GPIO pin : PA6 */
 
 GPIO_InitStruct.Pin = GPIO_PIN_6;
 
 GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;
 
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
 
 
 
 /*Configure GPIO pins : PB4 PB5 */
 
 GPIO_InitStruct.Pin = GPIO_PIN_4|GPIO_PIN_5;
 
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 
 HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
 
 
 
 /* EXTI interrupt init*/
 
 HAL_NVIC_SetPriority(EXTI9_5_IRQn, 0, 0);
 
 HAL_NVIC_EnableIRQ(EXTI9_5_IRQn);
 
 
 
}
 
 
 
/* USER CODE BEGIN 4 */
 
 
 
/* USER CODE END 4 */
 
 
 
/**
 
 * @brief This function is executed in case of error occurrence.
 
 * @retval None
 
 */
 
void Error_Handler(void)
 
{
 
 /* USER CODE BEGIN Error_Handler_Debug */
 
 /* User can add his own implementation to report the HAL error return state */
 
 __disable_irq();
 
 while (1)
 
 {
 
 }
 
 /* USER CODE END Error_Handler_Debug */
 
}
 
 
 
#ifdef USE_FULL_ASSERT
 
/**
 
 * @brief Reports the name of the source file and the source line number
 
 * where the assert_param error has occurred.
 
 * @param file: pointer to the source file name
 
 * @param line: assert_param error line source number
 
 * @retval None
 
 */
 
void assert_failed(uint8_t *file, uint32_t line)
 
{
 
 /* USER CODE BEGIN 6 */
 
 /* User can add his own implementation to report the file name and line number,
 
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 
 /* USER CODE END 6 */
 
}
 
#endif /* USE_FULL_ASSERT */

This topic has been closed for replies.
Brian TIDAL
Brian TIDALBest answer
ST Technical Moderator
March 21, 2023

Hi,

calling NDEF_WriteNDEF or NDEF_ReadNDEF before the various initialization cannot work.

I would suggest to have a look to MX_NFC7_Init and to customize it to fit with your needs.

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

2 replies

Brian TIDAL
Brian TIDALBest answer
ST Technical Moderator
March 21, 2023

Hi,

calling NDEF_WriteNDEF or NDEF_ReadNDEF before the various initialization cannot work.

I would suggest to have a look to MX_NFC7_Init and to customize it to fit with your needs.

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Schuyler
SchuylerAuthor
Associate III
March 22, 2023

Hi,

I know what you mean and I've been to see it. If I insert NDEF_WriteNDEFand NDEF_ReadNDEF after MX_NFC7_Init such as between/* USER CODE BEGIN 2 */ and /* USER CODE END 2 */, Can I enable the phone to read and write NDEF messages?

​