cancel
Showing results for 
Search instead for 
Did you mean: 

X-NUCLEO-53L1A2 board doesn't work with VL53L1_GUI. Center is no problem, but other sides (not only LEFT but also RIGHT) didn't work. I purchased two connectors (2x5 box) and soldered them on the board. I connected breakout boards to LEFT and RIGHT.

TYomo
Associate II

If I selected CENTER, the measurement started well. But if I selected LEFT or RIGHT, the measurement seemed to be stopped even though start button was pushed.

Is it bug?

1 REPLY 1
John E KVAM
ST Employee

Heck yes, it's a bug. We are working to get it fixed. Thanks for pointing it out.

(I'm guessing few people actually use the satellites or if the do, they don't complain much.)

We will get it fixed asap.

  • john

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question. It helps the next guy.