2021-03-22 03:26 PM
/* Private variables ---------------------------------------------------------*/
UART_HandleTypeDef huart2;
UART_HandleTypeDef huart4;
...
//#define UART_MODE 1
#define UART_MODE 2
...
#define USARTX USART4
#define huartX huart4
uint8_t UART_rxBuffer[50] = {0};
...
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{
uint8_t tstBuffer[] = "return: ";
HAL_UART_Transmit(&huartX, tstBuffer, strlen(tstBuffer), 100);
HAL_UART_Transmit(&huartX, UART_rxBuffer, 1, 100);//resend first byte
delay(10);
//normally: first enable interrupt again
HAL_UART_Receive_IT(&huartX, UART_rxBuffer, 1);
}
...
int main(void)
{
...
MX_USART2_UART_Init();
MX_USART4_UART_Init();
...
if (UART_MODE == 2)
{
//expect at least 4 chars --> 40 bytes --> better just one byte (stable)
HAL_UART_Receive_IT(&huartX, UART_rxBuffer, DATA_LENGTH_POLLING);
}
while (1)
{
// LED on
WRITE_REG(GPIOA->BSRR, GPIO_BSRR_BS_5);
//delay(500);
puts("Hello");//standard output redirected
char number_str[10];
sprintf(number_str, "%d", testCounter);
puts(number_str);
testCounter++;
/**
polling problem: after some data received will not work anymore!
*/
if (UART_MODE == 1)
{
//1a) polling --> needs fixed data length of transmission!!
//aa) reacts only on exact size!!
//ab) reacts once one too much data, afterwards it dies! //PROBLEM, stops when too much data was received!
HAL_StatusTypeDef res = HAL_UART_Receive (&huartX, UART_rxBuffer, DATA_LENGTH_POLLING, 5000);
if(res == HAL_OK) //why does it not work with USART4??
{
if (UART_rxBuffer[0] != '\0')
{
HAL_UART_Transmit(&huartX, UART_rxBuffer, 12, 100);
}
}
else if(res == HAL_TIMEOUT)
{
puts("timeout\n");
}
else if(res == HAL_BUSY)
{
puts("busy\n");
}
//1c) DMA --> needs added DMA channel
//HAL_UART_Receive_DMA (&huart4, UART1_rxBuffer, 12);
}//end polling
else//no uart polling
{
delay(500);
}
// LED off
WRITE_REG(GPIOA->BSRR, GPIO_BSRR_BR_5);
}
}
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};
/** Configure the main internal regulator output voltage
*/
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_BYPASS;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLMUL = RCC_PLLMUL_12;
RCC_OscInitStruct.PLL.PLLDIV = RCC_PLLDIV_3;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)
{
Error_Handler();
}
PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_USART2;
PeriphClkInit.Usart2ClockSelection = RCC_USART2CLKSOURCE_PCLK1;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
{
Error_Handler();
}
}
static void MX_USART2_UART_Init(void)
{
huart2.Instance = USART2;
huart2.Init.BaudRate = 115200;
huart2.Init.WordLength = UART_WORDLENGTH_8B;
huart2.Init.StopBits = UART_STOPBITS_1;
huart2.Init.Parity = UART_PARITY_NONE;
huart2.Init.Mode = UART_MODE_TX_RX;
huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart2.Init.OverSampling = UART_OVERSAMPLING_16;
huart2.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
huart2.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
if (HAL_UART_Init(&huart2) != HAL_OK)
{
Error_Handler();
}
}
static void MX_USART4_UART_Init(void)
{
huart4.Instance = USART4;
huart4.Init.BaudRate = 115200;
huart4.Init.WordLength = UART_WORDLENGTH_8B;
huart4.Init.StopBits = UART_STOPBITS_1;
huart4.Init.Parity = UART_PARITY_NONE;
huart4.Init.Mode = UART_MODE_TX_RX;
huart4.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart4.Init.OverSampling = UART_OVERSAMPLING_16;
huart4.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
huart4.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
if (HAL_UART_Init(&huart4) != HAL_OK)
{
Error_Handler();
}
}
2021-03-22 03:30 PM
btw
USAR2: I use the nucleo eval board with STLINK. -.-> sending receiving works
USAR4: usb to uart adapter --> only sending from uc works. Data send from PC not received.
Using 115200 baud rate
2021-03-22 03:58 PM
What hardware?
Read out and check the relevant GPIO registers for given pin.
Try to connect it to the STLink UART.
JW
2021-03-22 04:44 PM
2021-03-23 12:45 PM
STM32L073 nucleo board.
The Port config was done in Cube IDE, the right AF was chosen.
I can send from nucleo via USART2 and USART4, BUT only on USART2 also receiving data from PC.
Using exactly the same code when switching from USART2 to USART4.
void HAL_UART_MspInit(UART_HandleTypeDef* huart)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
if(huart->Instance==USART2)
{
/* USER CODE BEGIN USART2_MspInit 0 */
/* USER CODE END USART2_MspInit 0 */
/* Peripheral clock enable */
__HAL_RCC_USART2_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
/**USART2 GPIO Configuration
PA2 ------> USART2_TX
PA3 ------> USART2_RX
*/
GPIO_InitStruct.Pin = USART_TX_Pin|USART_RX_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF4_USART2;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/* USART2 interrupt Init */
HAL_NVIC_SetPriority(USART2_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(USART2_IRQn);
/* USER CODE BEGIN USART2_MspInit 1 */
/* USER CODE END USART2_MspInit 1 */
}
else if(huart->Instance==USART4)
{
/* USER CODE BEGIN USART4_MspInit 0 */
/* USER CODE END USART4_MspInit 0 */
/* Peripheral clock enable */
__HAL_RCC_USART4_CLK_ENABLE();
__HAL_RCC_GPIOC_CLK_ENABLE();
/**USART4 GPIO Configuration
PC10 ------> USART4_TX
PC11 ------> USART4_RX
*/
GPIO_InitStruct.Pin = GPIO_PIN_10|GPIO_PIN_11;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF6_USART4;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
/* USART4 interrupt Init */
HAL_NVIC_SetPriority(USART4_5_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(USART4_5_IRQn);
/* USER CODE BEGIN USART4_MspInit 1 */
/* USER CODE END USART4_MspInit 1 */
}
}
2021-03-23 01:44 PM
Read out and check the relevant GPIO registers for given pin.
Try to connect it to the STLink UART.
JW
2021-03-23 01:45 PM
thx Tesla DeLorean + Jan
I changed the solder bridges on my nucleo board to disconnect fixed USART2 from ST-Links virtual com port.
Connecting USART4 works there.
When I using different USB Uart adapter (FTDI chip) like this one
https://www.amazon.de/Serial-Konverter-Modul-original-FT232RL/dp/B075N82CDL
my uc will not receive data... just sending works.
Is there anything special I need to configure??
2021-03-23 01:52 PM
2021-03-23 02:09 PM
Follow up question:
either in polling or in interrupt mode when more data is send than expected the functions
will lead to the problem that no more data receiving will work...
Example below shows that expected length is 10 bytes, but user sends 11 bytes. Two times this works, but afterwards the UART_Receive is not working anymore.
Example: 1234567890received: 1234567890received: 12345678901received: 12345678901received: 123456789011234567890112345678901
What's the reason for that?