cancel
Showing results for 
Search instead for 
Did you mean: 

How can I duplicate the example binary from FP-SNS-MOTENVWB1?

ASmit.4
Associate II

I am trying to get quick-started with the following:

STM32WB55 - Nucleo Pack

X-Nucleo-IKS01A3 (MEMS Inertial and Environmental Expansion Board)

Stm32CubeIDE v 1.6.0

STBLESensor (Phone app)

FP-SNS-MOTENVWB1 v.1.0.0

To start, I've flashed the provided binary from the function pack (

STM32CubeFunctionPack_MOTENVWB1_V1.0.0\Projects\P-NUCLEO-WB55.Nucleo\Applications\MOTENV1\Binary\MOTENV1_IKS01A3_WB55RG.bin )

onto my nucleo board, and that works as expected. I can pair with the board via BLE and view the output on my phone app.

However, when I build and flash the project from CubeIDE, I don't get the same results.

I created a new project from the Cube MX configuration file provided in the Function pack at \STM32CubeFunctionPack_MOTENVWB1_V1.0.0\Projects\P-NUCLEO-WB55.Nucleo\Applications\MOTENV1\MOTENV1_IKS01A3_WB55RG.ioc

I get a warning that the project was set-up using Cube firmware version 1.2.0 and gives me the option to either migrate or continue. I have tried both options at this point.

I build the project. copy the project binary to the board and... nothing.

What step am I missing to get this working so I can move on with development?

0 REPLIES 0