2021-03-15 12:10 PM
I am trying to make some tests with the touchGFX and the STM32H7B3I-DK kit.
I have tried different approaches with online step by step videos and webinars.
This one: https://www.youtube.com/watch?v=4-fyx4e96jk
I have tried now and all compiles and uploads without error, but the display does not turn on. It works because uploading something simple directly from tGFX designer turn on the display.
I get 1 warning, but don't know why that should have impact on the display not turning on. The warning is:
Invalid project path: Include path not found (C:\TouchGFXProjects\Designer_tGFX_1\Middlewares\Third_Party\FreeRTOS\Source\CMSIS_RTOS).
Why should that meke the display stay black, and what should I do to get rid of the warning. I have followed the video to the point.
I have read at some places that this board is not as good as others regarding "Working right of the shelf"
Another thing: If I try to flash the original demo into it, there is a lot of tear in the images on the mainscreen. Why is that?
Solved! Go to Solution.
2021-03-24 11:45 PM
Well, gave it another go, and voila finally 4 weeks of intense work paid off. 🙂
I based my experience on the guide mentioned in the start of this thread. https://www.youtube.com/watch?v=4-fyx4e96jk
Now got it working with:
CubeMX 6.2.0 with MCU package STM32Cube_FW_H7_V1.9.0
CubeIDE 1.6.0
touchGFX 4.16.1
The black screen happened because there is a mismatch somewhere if using FW_H7_V1.6.0 instead of FW_H7_V1.9.0.
Apparently Designer generates as if the default was FW 1.6.0. But there is a fix for this in the CubeMX. In the project setup (when a project is loaded), Default Firmware Location should be unticked and you should browse to the location of the resent version (here 1.9.0).
Some of the other stuff I had to struggle with, was just 2 typos of my own.
Sometimes the flashing stopped in the middle of flashing. The only solution for me was to reset the board and try again, and sometimes it was also necessary to "make clean" the project and start a new compilation.
2021-03-15 05:59 PM
Hello BJens.1,
First to reassure you, your warning has no effect on your board's behavior. Basically, you have a non existant folder called CMSIS_RTOS. The right folder is CMSIS_RTOS_V2 and is also included. This is why it compiles correctly anyway. To remove it, I need to know what IDE you are using but basically, you need to go to your project settings and remove the include path for CMSIS_RTOS.
As for why it is black, they can be many reasons for this.
Have you tried the following steps ? :
/Alexandre
2021-03-15 11:38 PM
Yes. no matter which example I choose from the designer, I compile and run on the target everything is ok. And all is looking pretty good I might add. But I think the problems arise, at least with this board, when trying to use the hardware with the tGFX. And that must be the whole purpose of a controller. =)
Oh and by the way, it is a fresh install (yesterday) So it is all the latest tools.
tGFX 4.16.1
CubeMx 6.2.0
CubeIDE 1.6.0
2021-03-16 01:23 AM
I haven't seen the video so the below suggestions might not be valid for your case, but with that said the usual culprits when the screen stays black are two things.
a third but less likely option could be the back-light not being turned on but that usually works with the default hardware settings.
2021-03-16 02:15 AM
Thanks for you reply. In the video he shows the kit working with backlight on after doing the steps I have mimiked. So following a step-by-step with the same kit, and nothing working as expected is pretty disappointing. :(
Well in these pandemic times, I'm working from home, so no access to an oscilloscope, to meassure any pins actual state.
And all is very overwhelming right now, it's a steep learning curve. I'm used to C but C++ is pretty new to me. Have read a lot about it, but never yet made a project in C++. And have to get familiar with the IDE - never used eclipse before. And have only experience with 8 bit AT-MEGA controllers from Atme. But we want to step up our game and enter the bright and exciting world of 32 bits and all the fantastic projects that now become possible. 🙂 Even though HAL is a layer to remove complexity, it is at the same time introducing another layer of complexity. So a lot of new things to get into. 🙂
If anything is missing, it should have been mentioned in the video I guess.
2021-03-16 02:38 AM
Hi,
I also faced a black display issue when generating code with CubeMX 6.2 for the H7B3-dk board, I havent investigated yet on it but I would advise to install CubeMX 6.1.1 for now to see if it fixes your issue.
/Romain
2021-03-16 02:40 AM
Hello BJens.1,
I'm sorry to hear that.
Thank you for your feedback. It is actually very useful to hear your struggles and from where you come (C programmer experienced with 8 bit MCUs). This helps us understand what kind of people are trying to use TouchGFX and ST softwares in general and try to find ways to help making the ecosystem more user-friendly.
What I usually suggest and what I did when I started with TouchGFX was to compare existing working code with my own and see/analyze the discrepancies.
So to understand more I would recommend you to compare your project with the Application Template H7B3-DISCO available in TouchGFX Designer and see what's different.
You can also share your project in this thread. I can't guarantee I will have much time to look deep into it but we never know. Also, someone else could have a look and help you too. This is what the community is for ^^
/Alexandre
2021-03-16 03:41 AM
Ok, that changed the black display, so now it shows me the 2 screens. The hardware part with the LEDs and the button does not, but I will play a little with that and return.
In the meantime I can tell, that it is not just uninstalling the CubeMX 6.2.0 and installing CubeMX 6.1.1. Because when you start up the CubMX 6.1.1 it will not read the *.ioc file because it i generated with a newer version. So the choises are to either start from scratch, or do as I did. Open the *.ioc file in notepad or something similar, find the line where the CubMX version is mentioned, and change it to the version you use (in this case 6.1.1) and try to open the ioc again and generate the code from within there again. And then when opening the project in CubeIDE the projekt can compile and flash - and it works (Well sort of, but I have to investigate if all my variables are named correctly and so on).
I know it is not the right way to edit the *.ioc file, because if something in the way it is generated has changed from version to version, it could give me some other problems. But in this case it seems to work. 🙂
2021-03-16 05:59 AM
Ok went through all the code added in the example, ending up with the same result as all the other times I have tried different tutorials. No functionality. The display shows the items (the same way as in tGFX designer) but no functionality. Which I guess is not the purpose of the tutorials.
The tutorials should be able to guide newbees into the faboulous world of these controllers, not make us descuriaged and upgiving. :(
We (I) need some tutorials up-to-date with the newest software packages (because those are the ones beginners download), which are worked through examples tested and proven to work.
And I'm absolutely not writing this because I'm not happy with te tools. But they should work for a beginner without all kind of workarounds.
I am thrilled about the tools, they seem to be very good (and free - lets not forget), but if I should be convinced that I have landed in the right (processor) family, I need some good experiences to convince me. 🙂
When I get this to work I have a ton of additional questions. 🙂
2021-03-16 06:51 AM
Yeah I was wrong CubeMX 6.2 is not the main issue as it appears with 6.1.1 as well, it is the FW package selected. CubeMX does not recognize that the fw package v1.6. is not the latest one. You have to go in CubeMX in the Project manager tab in the "Mcu and firmware package" section. You have to uncheck the "Use default firmware location" and browse to the v1.9.0 folder.
I have reported this to the CubemX team. This is a very weird issue as v1.6.0 used to work. Unfortunately it is out of our reach for now, we will try to update the application templates for the h7b3 disco board asap in order to fix this problem for now.
/Romain