2021-03-09 05:37 AM
Hello,
I've a strange problem with CubeIDE 1.6.0, there's no binary or hex file output even if the corresponding outputs are activated under MCU post build outputs. Any ideas what might be the issue there?
Regards
Solved! Go to Solution.
2021-04-08 02:02 AM
External builder is the recommended way in CubeIDE as in many other Eclipse/CDT based tools. We chose External rather than Internal because it was more actively support by the Eclipse community and it makes sense to move with the OSS community. So, please consider Internal Builder untested by us, so things like hex/bin/srec generation may not be supported at all.
Thanks @Cartu38 OpenDev for creative work-arounds! 😉
2021-03-09 09:14 AM
2021-03-09 09:20 AM
Same here, after importing Atollic projects to v. 1.6.0
Has to use a post-build script for binary file. Are your projects imported?
-- pa
2021-03-09 11:58 PM
@Community member
The map and elf files are created well. Which log files do you mean?
@Pavel A.
No, I didn't import the project. It was made with CubeIDE 1.5.x and F4 HAL v1.25.2. Then I updated to CubeIDE 1.6.0 and F4 HAL 1.26.0 a few days ago.
I'm not sure if I activated the binary file output when the project was created, so I can't say for sure that it's related to the CubeIDE or the F4 HAL update.
Regards
2021-03-10 08:59 AM
While they are pondering on yet another problem , here is a postbuild script to plug the hole.
For Linux _and_ Windows. Not tested on OSX.
-- pa
#!/bin/sh
# Add this command as postbuild action:
# sh postbuild.sh ${BuildArtifactFileBaseName}
EXENAME=$1
[ "$HOMEDRIVE" = "" ] || BUSYBOX="busybox "
# Print memory sizes:
arm-none-eabi-size $EXENAME.elf || exit 1
# Convert to bin
arm-none-eabi-objcopy -O binary $EXENAME.elf $EXENAME.bin
# and print size of the .bin
$BUSYBOX stat -L -c "%N size=%s" $EXENAME.bin
# Produce .list :
arm-none-eabi-objdump -h -S $EXENAME.elf > $EXENAME.list
echo "POSTBUILD DONE"
2021-03-22 12:57 PM
It appears that the MCU Post build outputs step is run only when Builder Type (on Builder tab in Properties->C/C++ Build) is External builder. When I set Builder Type to Internal builder, the MCU Post build outputs step is not run.
This appears to be a bug in STCubeIDE 1.6.0
2021-03-23 12:55 AM
Hello @DShan.1 ,
thank you for reporting it. I hope ST will take notice of this issue.
Regards
2021-03-23 01:30 AM
Fact is STM32CubeIDE default is external builder not internal one.
I confirm if internal builder usage post build step leading to have following UI settings not active
But still possible if internal builder to rely by yourself on post build steps
Why are you moving to internal builder ???
2021-03-23 06:31 PM
> Why are you moving to internal builder ???
It just feels cleaner, does not litter all these makefiles and does not run external make program.
Though recently ST supplies improved version of make and other gnu tools for Windows, that support very long paths.
So maybe there's no longer a reason to use internal builder.
--pa
2021-04-07 05:56 AM
This issue does not appear to have been resolved in the just released update to STM32CubeIDE, version 1.61.