2021-03-05 09:56 AM
2021-03-05 11:01 AM
Open STM32CubeMX
Either of these
Then:
Paul
2021-03-05 01:02 PM
2021-03-05 01:06 PM
If you keep the chipselect pins high, all other pins (maybe except dedicated output such as interrupt pin, if the LCD has such) can be considered as free.
JW
2021-03-09 07:27 AM
Another proposal when using STM32CubeMX with Board Selector: go to Pinout tab and click on "Clear Pinouts":
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2021-03-09 08:25 AM
but as the LCD is ON, for instance, also if I change the features of the PINs, when I'm doing the connections the pins are always connected with the LCD pins and the outside. I was wondering if this can create interference. The answer of @Community member seems satisfatory, as I'm going to disable the chip via the chipset. Or are you suggesting that is enough to delete the features and add the new features?
Anyway, thanks for your answers
2021-03-09 08:28 AM
@Community member is suggesting just to disable/add the features on the desidered pin. I think that your answer is more correct ( disable the chips select) but what do you think of simply disabling the PIN (I think that there should be some interference, but I'm not sure).
Thanks in any way for your answer.
2021-03-09 08:41 AM
By setting the pins on STM32 which are connected to the chipselects, to GPIO Out and high, you make sure that data lines of the LCD controller and the SDRAM will never turn to output, potentially conflicting with the pins on STM32 to which these data lines are connected.
Address lines should be OK, they are input only.
A closer examination of SDRAM and LCD controller datasheet might reveal further details.
JW
2021-04-30 08:48 AM
thanks for your useful answer