cancel
Showing results for 
Search instead for 
Did you mean: 

How to install POWERSTEP01 library in STM32CubeMx Project ?

LHerm.1
Associate III

Hello everyone, I'm using the evaluation board of the motor driver POWERSTEP01 (EVLPOWERSTEP01) with a nucleo board NUCLEO-F401-RE. I want to know how to integrate this library in a classic project STM32 cubeMX IDE. I find the libray included in a "Hello world" Project but the problem is that i have to program my board via ARM mbed.

But, i want to use this library in a STM32 cubeMX project ... So my questions is : How to includes the right files of this library to be able to use its functions? 

You can see two picture : the first one show where the library is, and the second show were i want to include it.

This is the Mbed interface where the library is (There are a lot of files and I don't know which ones to take)

0693W000007ZtUsQAK.pngAnd this is where i want to includes the right files to program my board via STM32CubeMX

0693W000007ZtVCQA0.png 

I have tried to be as clear as possible, Thank for your help 

1 REPLY 1
Laurent Ca...
Lead II

Dear @LHerm.1​ 

Does this library have any dedicated documentation?

Best regards

Laurent Ca...