2021-03-01 10:50 PM
Hi,
I am working with STM32L4S5ZI MCU and I have a custom board with the same.
I am evaluating the hardware timer and as part of my project I need time in nano seconds for some time constrained work. Right now I am using Timer3 and below is my sample code with which I am able to get the counter value between a start and stop of the timer.
Can I derive the time with nano second precision using these timers on the chip? And I need to do this specifically with a timer and not using any other means like a DWT.
Please let me know if there is a way to do this. Thanks a lot.
int i =1;
regValue = TIM3->CNT;
printf("Timer value %d\n", regValue);
HAL_TIM_Base_Start(&htim3);
printf("Timer cycle %d\n", i);
i++;
HAL_TIM_Base_Stop(&htim3);
regValue = TIM3->CNT;
printf("Timer value %d\n\n", regValue);
2021-03-02 02:59 AM
Timer resolution is limited by the timer clock Maximum clock is 120 MHz, so you get 8.33 ms resolution.
2021-03-02 03:20 AM
Hi Uwe Bonnes,
Thank you for your response. I figured out the max clock as 120MHz just after posting the above question.
As per your response, the resolution for a 120MHz clock should be 8.33ns rather than 8.33ms right?
Thanks!
2021-03-02 03:29 AM
Off by one typing...
2021-03-02 03:35 AM
If what you want to do is measure the time in nanoseconds in between events (for example width of a digital pulse)
you should take a look at the INPUT CAPTURE funcionality
and maybe use the timer with 0 preescaler and max clock speed
2021-03-02 04:12 AM
Just to confirm what you mean by "Off by one typing" is that you pressed m instead of n right? 🙂
2021-03-02 04:26 AM
Just wanted to add to the question,
so the max Period that can be set to TIM3 is 65535 since it is a 16bit timer. So once the period is completed I can see that the counter restarts from 0.
Now how can I keep track of the number of times that the period got completed so that at the final calculation I can calculate the entire time?
Sharing something on this would be really helpful. Thanks!
2021-03-02 07:06 AM
Use Timer overflow interrupt and count overflows. Be carefully when combining overflow count and timer count to a number > 16 Bit!
2021-03-02 08:19 PM
That sounds good.
order to use the interrupts, I should start and stop the timer with interruption right?
HAL_TIMx_BaseStart_IT()
HAL_TIMx_BaseStop_IT()
2021-03-02 11:34 PM
Hi Uwe,
Checkout my below test code, with this I dont see that the callback function
void HAL_GetTimerOverflow_Count(struct __TIM_HandleTypeDef *);
int main(void)
{
/* USER CODE BEGIN 1 */
uint32_t regValue;
uint8_t cycles;
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
MX_GPIO_Init();
MX_TIM3_Init();
HAL_TIM_Base_Start_IT(&htim3);
TIM3->DIER = TIM_DIER_UIE_Msk;
while (1)
{
regValue = TIM3->CNT ;
printf("Timer value %d\n", regValue);
for(int i=0; i<100000; i++);
if(overflowCount_g > 0) {
HAL_TIM_Base_Stop_IT(&htim3);
regValue = TIM3->CNT;
HAL_CalculateTime(regValue);
}
// printf("Timer value %d\n\n", regValue);
}
/* USER CODE END 3 */
}
void HAL_GetTimerOverflow_Count(struct __TIM_HandleTypeDef *htim)
{
overflowCount_g += 1;
}
is executed but I can see that the counter finished counting till 65535 and started recounting. I have enabled the Update Interrupt in the DIER register. In the call back function I am incrementing a global variable and checking the value to be more than 0 in while loop. But if I put a breakpoint in callback function, I never see that breakpoint being hit.
I have also set the USE_HAL_TIM_REGISTER_CALLBACKS in stm32l4xx_hal_conf.
Is there anything wrong in what I am doing?
Please let me know what do you think
Thanks