2021-02-22 07:42 AM
Hi, i find myself wanting to use stm bootloader instead of having to code my own.:|
My setup consists in 4 identical nodes hooked up to a 2m long canbus.
I found this note in the AN3154 appnote
I dont use more than one node at a time....
Solved! Go to Solution.
2021-02-28 11:41 PM
from ST support:
Description: Hello, unfortunately the CAN bootloader is designed for use cases where other CAN nodes are not active, which is not suitable for some application. I'm afraid the customer would have to write their own bootloader, or some how temporarily disable the other nodes on the bus. We don't have example for CAN bootloader, but we do for UART: https://www.st.com/content/st_com/en/products/embedded-software/mcu-mpu-embedded-software/stm32-embedded-software/stm32cube-expansion-packages/x-cube-iap-usart.html
So it might be useful for customer as reference.
Best regards, @Adam BERLINGER
2021-02-22 08:47 AM
>>i find myself wanting to use stm bootloader instead of having to code my own.
At that point you have little control of the situation, best not to be beholden to the design choices of others..
Can you clamp the unused nodes in reset whilst using the ST system loader? Or gate the transceiver with the BOOT0 or NRST pins?
2021-02-22 09:06 AM
>>At that point you have little control of the situation, best not to be beholden to the design choices of others..
I find the stm bootloader very well documented and already factory flashed (it doesnt eat up memory and works out of the box) so its just convenient for me.
Or so i tought.... i believe there is some canbus ACKing and NACKing silly logic behind my bug.
>>Can you clamp the unused nodes in reset whilst using the ST system loader? Or gate the transceiver with the BOOT0 or NRST pins?
My backup plan was disabling every other canbus for 30 seconds and enabling them again (hardware) but i want to fight this trough a bit more.
2021-02-22 09:12 AM
I just found another person with my same bug two years ago.
And while sniffing the bus i think i figured it out, for some silly reason the bootloader is expecting the first 0x79 command to be NACKED and only after that reply to the next 0x79 command.
If you send the 0x79 only once (automatic resend disable) the bootloader doesnt work either
2021-02-28 11:41 PM
from ST support:
Description: Hello, unfortunately the CAN bootloader is designed for use cases where other CAN nodes are not active, which is not suitable for some application. I'm afraid the customer would have to write their own bootloader, or some how temporarily disable the other nodes on the bus. We don't have example for CAN bootloader, but we do for UART: https://www.st.com/content/st_com/en/products/embedded-software/mcu-mpu-embedded-software/stm32-embedded-software/stm32cube-expansion-packages/x-cube-iap-usart.html
So it might be useful for customer as reference.
Best regards, @Adam BERLINGER