cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX SPI1 Missing CS on PD14. (Arduino-Header D10 on Nucleo-H743ZI (MB1137))

Grisby
Associate II

I use Nucleo-H743ZI and want use the Aduino-Header. On Board MB1137 PIN D10 (CS) is conneted to PD14. In CubeMX SPI1 NSS1 is set to PA4. I can not change to PD14, because there is no SPI1_CS in PD14 in CubeMX. How can I fix this?

I don't want change the source code after every generate.

1 REPLY 1
Houssem CHAABANI
Senior II

Hi @Grisby​ ,

Thank you for these details.

Could you share your .ioc file to check this issue ?

Thanks