2021-02-19 11:28 PM
Hello everyone,
I am currently working over stepper motor with STM32F7 series controller and i'm trying to control the stepper using PWM timers. Somehow there is no such support for the same as all i found is controlling servo motor or some other related searches. Main issue is i already created PWM and i can see it over Pins using oscilloscope but when i connect my motor it ain't move a bit, not even vibration which shows that nothing is happening through PWM. I would like to know about how to control motor using PWM. If anyone can help me from scratch that would be a great help.
2021-02-20 01:23 AM
Supposed you have a proper motor driver, I would start generating pulses by bit-banging in software, using the same pins in GPIO output mode.
2021-02-21 08:21 PM
Yes, i have a motor driver IC, and i did rotated motor by bit banging, using the same pins in GPIO output mode. but now i want to control it with PWM using timers. so all i need is to know the concept, as the all i understood by reading web searches and related documents is that i've to change its duty cycle to create a sine-wave, but i don't understand how it will make it run.
2021-02-22 12:52 AM
As I don't know the type of motor and driver chip you are using, here are some general remarks: There is an app note "AN2820 Driving bipolar stepper motors..." explaining different types of stepper motors. There is also an accompanying firmware, but I don't know how uselful that is for you.
> that i've to change its duty cycle to create a sine-wave
The basic code pattern is:
/* USER CODE BEGIN 2 */
#define N 1000
static uint16_t pwm[N];
for( int i=0; i<N; ++i ) {
pwm[i] = 500 + 490*sin( (2*3.14159 * i)/N ); // one sine period
}
HAL_TIM_PWM_Start_DMA(&htim2, TIM_CHANNEL_2, (uint32_t*)pwm, N);
/* USER CODE END 2 */
(Any other pattern you need for the pwm will do as well.)
Configure TIM2 Channel 2 in PWM mode and set Trigger Event to OC2REF. Enable TIM2CH2 circular DMA with half-word -> word transfers from mem to device.
If you need to specify each edge independently, set Timer Channel to OC Toggle mode, use HAL_TIM_OC_Start_DMA and an array with monotonically increasing timestamps for the edges.
hth
KnarfB
2021-03-19 11:09 PM
I guess this helps me lil bit as now on i can rotate motor without skipping any step and smoothly. The point is when i was changing the duty cycle of timer i missed a part in reference manual where it describes that the PWM pulse value should be equal to the period value, above that value will be count as 100% duty which causing issue in my case. Moreover there is more thing that effects is the combination of +2 -2 and -1 +1 will be in sequence always, as i was missed that part the motor moves but skip steps. hence remembering these points i solved my issue. Thanks for you help that SINE look up table helped me alot.