cancel
Showing results for 
Search instead for 
Did you mean: 

I have STM32CubeIDE 1.5.1 installed. There is no option for File >> New STM32 Project. How then do I create a new STM32 Project from within STM32CubeIDE? Thx, Hab

Hab Collector
Associate II
 
4 REPLIES 4
Julien D
ST Employee

How did you installed the version 1.5.1, is it a fresh installation or an update from previous version?

Did you already installed third-party plugins such as git?

Asking this because you could be in the same situation than https://community.st.com/s/question/0D53W00000S5KhZSAV/error-unknown-nature-on-stm32cube-ide-after-update

Hab Collector
Associate II

This was an update not a fresh install. I have not installed git to STM32CubeIDE, but it is installed for Atollic. I am using Windows 10. I took a look at the link - not sure that is the issue I am having, does not read like my situation, but it could be related. Would you suggest an uninstall and fresh install?

Julien D
ST Employee

To confirm or not the issue from the other thread could you start STM32CubeIDE using "stm32cubeidec.exe -consoleLog" and paste here the startup log ?

Hab Collector
Associate II

Sorry for the delay. Apparently the problems are one and the same. I updated the JRE as you suggested in the link https://community.st.com/s/question/0D53W00000S5KhZSAV/error-unknown-nature-on-stm32cube-ide-after-update and that appears to have corrected the issue. Much thanks.