2021-02-03 06:15 AM
Hello,
When activating STM32_WPAN in STM32CubeIDE for STM32WB, the prescaler of RTC is forced to CFG_RTC_ASYNCH_PRESCALER (value is 15) and CFG_RTC_SYNCH_PRESCALER ( value is 0x7FFF ).
I am used to configure RTC on other STM32 products with 127 and 255 values.
During test, I see that the RTC is running ~ 16 times to slow.
Do I miss something?
Is this problem similar to point 2 of the question "STM32WB - Problems with BLE and RTC" from "MLind.2" on 2020∕05∕25?
Thanks for help
Best regards
Paul
2021-02-08 10:15 AM
Additional questions to the problem:
Why is the prescaler of RTC forced to only the defines?
In source code generated from STM32CubeIDE, (file app_conf.h line 333) I can read:
#define CFG_RTCCLK_DIVIDER_CONF 0
#if (CFG_RTCCLK_DIVIDER_CONF == 0)
/**
* Custom configuration
* It does not support 1Hz calendar
* It divides the RTC CLK by 16
*/
#define CFG_RTCCLK_DIV (16)
#define CFG_RTC_WUCKSEL_DIVIDER (0)
#define CFG_RTC_ASYNCH_PRESCALER (CFG_RTCCLK_DIV - 1)
#define CFG_RTC_SYNCH_PRESCALER (0x7FFF)
#else
To use RTC together with STM32_WPAN (I hope that these are usable together), should I modify app_conf.h?
Wouldn't it be better to be generated by STMCubeIDE?
How to do?
2021-04-10 04:16 AM
change #define CFG_RTCCLK_DIVIDER_CONF 0 to 16