cancel
Showing results for 
Search instead for 
Did you mean: 

Bug: STM32CubeMX code generation for STM32cubeIDE

SDeha.1
Associate

Hello,

I have some problem with the latest version of cubeMX (v6.1.1), it won't create a project file for STM32 (well I would like to use simulink with mat/target before using STM32cubeIDE that's why I use cubeMx and the project work with µvision),

the configuration of my project are :

target board : NUCLEO-F446RE

target IDE : STM32cubeIDE 1.5.1

here is my error :

0693W000007CqeeQAC.pngYou can find the log in attach the log (log_CubeMx.txt) which consist of one generation done the 27/01 at 12:08 and the configuration file .ioc (BilleSTM32.ioc).

Thank you for your future help.

S. Dehais

2 REPLIES 2
Khouloud ZEMMELI
ST Employee

Hello @Community member​ 

Thanks for your feedback, it will be internally checked.

I'll get back to you as soon as possible.

Khouloud

Cartu38 OpenDev
Lead II

Works like a charm on my side but possibly we are missing here some details about your running context.

Looking at your .log file sounds you've project on D:\. Where (which partition I mean) is STM32CubeIDE installed ? Where (which partition I mean) are your firmware repository set ? Are you using some special char or blank one as part of any of such path ?

... have already seen issue reported here Thanks such forum.