cancel
Showing results for 
Search instead for 
Did you mean: 

How to wire STEVAL-MKI197V1 to a muRata nRF development board: WSM-BL241-ADA-008DK.

BGrap.1
Associate

The STEVAL-MKI197V1 has standard breadboard pins on it. The muRata dk (WSM-BL241-ADA-008DK) has available connection points in position JP4 - looks like the right place to attach. Is there a ribbon cable or adapter to connect these two boards together?? thank you! (see photos)

1 ACCEPTED SOLUTION

Accepted Solutions
Eleon BORLINI
ST Employee

Hi @BGrap.1​ ,

the STEVAL-MKI197V1 -and in general the DIL24 connector of ST sensors' STEVALs- has been designed to be compatible with the STEVAL-MKI109V3 motherboard (and the X-Nucleo expansions for the Sensors).

I don't think that the schematics are immediately compatible, but if you could remap the functions of the muRata nRF according to STEVAL-MKI197V1 schematic, you could make the two boards compatible.

-Eleon

View solution in original post

2 REPLIES 2
Eleon BORLINI
ST Employee

Hi @BGrap.1​ ,

the STEVAL-MKI197V1 -and in general the DIL24 connector of ST sensors' STEVALs- has been designed to be compatible with the STEVAL-MKI109V3 motherboard (and the X-Nucleo expansions for the Sensors).

I don't think that the schematics are immediately compatible, but if you could remap the functions of the muRata nRF according to STEVAL-MKI197V1 schematic, you could make the two boards compatible.

-Eleon

BGrap.1
Associate

Thanks for the fast reply. We did see the DIL24 connector on the motherboard (STEVAL-MKI109v3) and considered that but thought we would reach out to anyone who might have manually wired them together.

thanks!

Brian