cancel
Showing results for 
Search instead for 
Did you mean: 

STEVAL-IME013V1 doesn't connect to Ultrasound Pulser Waveform Demo (STSW-IME011, Error code 2)

BSus.1
Associate

I have a STEVAL-IME013V1 Evaluation board (STM32 + STHV800) and want to program arbitrary pulse trains with the "Ultrasound Pulser Waveform Demo" (STSW-IME011) with Win10.

  • I connect the board via USB.
  • I press USR button (LED5 blinks orange) on the board and F5 in the Demo Program
  • I get the Error: Connection failed! Unable to retrieve the device type.
  • If I select the correct IC (STHV800) then I get Error Code 2
  • Reset RST doesn't help
  • Changing the baud rate doesn't help
  • Adding +5 V/-5 V doesn't help

Pictures of the error, the software version and the board are in the attachment.

Do you have any idea what to do?

Thank you

Best regards

Bjoern

Edit:

I tried it on an old Windows 7 Computer and it worked.

It seems to be a driver problem.

1 REPLY 1
TYong.3
Associate II

Hi,

I had the same issue and managed to get it working on Win10 by doing:

"Communication" > " Configuration" (F4) > Uncheck "Auto Discovery Board" > Connect manually (F5)

Hope it works for you too