cancel
Showing results for 
Search instead for 
Did you mean: 

X-CUBE-TOUCHGFX 4.16.0 is out

Romain DIELEMAN
ST Employee

Hi Everyone, the TouchGFX team wishes you a happy new year.

If you haven't noticed by now, X-CUBE-TOUCHGFX 4.16.0 is out, available from CubeMX 6.0+ and from st.com as a zip (Also installable through CubeMX).

Here is the documentation for 4.16.0: https://support.touchgfx.com/

Main features:

  1. Built in support for a Gauge widget
  2. New screen transition called "Block Transition"
  3. New invalidation algorithm for improved performances

You can see all the bug fixing and improvements in the changelog.

/Romain

32 REPLIES 32
m4l490n
Associate III

Are there any plans on releasing TouchGFX for Linux?​

Hi,

It is not part of our short term plan.

/Romain

What about TouchGFX for STM32MP157 ?

Like Embedded Wizard https://doc.embedded-wizard.de/getting-started-stm32mp157c-dk2?v=9.30

Hi,

I do not believe it is on our plan either as TouchGFX is aimed to run on MCUs not MPUs.

/Romain

Tuoman
Senior II

Plans to include the Base View class?

https://community.st.com/s/question/0D50X0000CBl27ZSQR/add-an-interaction-to-all-screens

This is my #1 needed feature. We have +50 views and counting, which all must have the same features (popup handler, hotkey window), which must be copied and pasted to all views. Base view would make the TouchGFX perfect tool in my eyes.

Hi,

we are working on it right now. I do not know the status nor potential delivery date unfortunately.

/Romain

Myurt.1
Associate

Hi,

Are there any plans to add STM32H745I DISCO support for TouchGFX? If yes, when will it be added?

Good question, I do not know what is the plan for the next boards to support. Maybe we should share it, I know that we are working on the H7b3 eval at the moment and dual core dev kits.

I do not see the STM32H745I DISCO in the short term planning but I will check with the Marketing team. maybe they will push for it.

/Romain

Ok so I asked around and it is in our plans, no estimated release date yet however.