2021-01-12 01:59 AM
Hello,
My simple application should read some configuration which I put by CubeProgrammer from 0x0800C800, I want to debug the application but seems the debugger erases the flash at all. Could you tell me please how to prevent full internal flash erasing when debugging?
Thanks
P.S.
MEMORY
{
DTCMRAM (xrw) : ORIGIN = 0x20000000, LENGTH = 128K
ITCMRAM (xrw) : ORIGIN = 0x00000000, LENGTH = 64K
RAM_D1 (xrw) : ORIGIN = 0x24000000, LENGTH = 512K
RAM_D2 (xrw) : ORIGIN = 0x30000000, LENGTH = 288K
RAM_D3 (xrw) : ORIGIN = 0x38000000, LENGTH = 64K
FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 25K
DATA (rx) : ORIGIN = 0x0800C800, LENGTH = 25K
}
2021-01-12 02:03 AM
2021-01-12 06:01 AM
Maybe, but how I can configure this?