cancel
Showing results for 
Search instead for 
Did you mean: 

Need StLinkV2.1 firmware for the STM32F7508-DK

VBurs
Associate II

Hi,

My St-link on board the STM32F7508-DK is corrupted and i cannot flash it over usb anymore.

I've manage to find a Stlink V2 binary and it works ok for flashing but not for debugging.

Also the V2 version does not have the ST-link in mass storage for drag and drop programmation.

Is it possible to provide the binaries to be able to flash the ST-link MCU with the STlinkV2.1 firmware version?

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

You can perform a firmware upgrade using e.g. the STM32CubeProgrammer.

If you can establish a connection to your DK with the buttons ST-LINK and Connect (top right), you should disconnect the connection again and click the blue update button Firmware in the bottom right. This opens the STLinkUpgrade program, in which you click on Open in update mode and after that on Upgrade (bottom left).

Good luck!

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Peter BENSCH
ST Employee

You can perform a firmware upgrade using e.g. the STM32CubeProgrammer.

If you can establish a connection to your DK with the buttons ST-LINK and Connect (top right), you should disconnect the connection again and click the blue update button Firmware in the bottom right. This opens the STLinkUpgrade program, in which you click on Open in update mode and after that on Upgrade (bottom left).

Good luck!

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Houda GHABRI
ST Employee

Hi @Community member​ ,

Hope your issue is fixed using the solution proposed by Peter, if not keep us informed.

Houda