cancel
Showing results for 
Search instead for 
Did you mean: 

"Attempt to unlock mutex that was not locked"

YEbne.1
Associate

I get the following error in terminal quite frequently which crashes the stm32cubeide. This usually happens when I am opening the ".ioc" file.

Attempt to unlock mutex that was not locked

This is my workspace folder if you are interested: https://github.com/yosoufe/ExperineceKemet/tree/master/cubews

I also sometimes see the following error message and then a crash

[xcb] Unknown sequence number while processing reply
[xcb] Most likely this is a multi-threaded client and XInitThreads has not been called
[xcb] Aborting, sorry about that.
java: ../../src/xcb_io.c:639: _XReply: Assertion `!xcb_xlib_threads_sequence_lost' failed.

I should run it via terminal to see the error. If I click on the icon, it crashes without any error message.

I am running it on Ubuntu 18.04 machine. Is there anyway to run the cubeIDE in safe mode to disable some plugins?

Thanks

3 REPLIES 3
DFedo.1
Associate II

Same here, release 1.7.0 and Cube keeps randomly crashing (way worse than previous releases), making it barely usable just for templates generation.

Cartu38 OpenDev
Lead II

@YEbne.1​ @DFedo.1​ googling a bit sounds like GTK issue. Which GTK version are you relying on ?

Are you relying on Xorg or Wayland ?

libgtk-3, up to date ubuntu 20.04 LTS, xorg