2020-12-15 01:02 AM
I'm using FirmwarePackage=STM32Cube FW_L1 V1.10.1
I'm looking at these functions in stm32l1xx_hal.c:
/**
* @brief Return the first word of the unique device identifier (UID based on 96 bits)
* @retval Device identifier 31:0 bits
*/
uint32_t HAL_GetUIDw0(void)
{
return(READ_REG(*((uint32_t *)UID_BASE)));
}
/**
* @brief Return the second word of the unique device identifier (UID based on 96 bits)
* @retval Device identifier 63:32 bits
*/
uint32_t HAL_GetUIDw1(void)
{
return(READ_REG(*((uint32_t *)(UID_BASE + 0x4U))));
}
/**
* @brief Return the third word of the unique device identifier (UID based on 96 bits)
* @retval Device identifier 95:64 bits
*/
uint32_t HAL_GetUIDw2(void)
{
return(READ_REG(*((uint32_t *)(UID_BASE + 0x14U))));
}
They do not use a volatile pointer. Shouldn't they? Could a compiler optimize this in a bad way?
I would write them as:
return *((__IO uint32_t *)UID_BASE);
2020-12-15 01:34 AM
2020-12-15 06:39 AM
But the IDCODE register is defined volatile and that doesn't either change?
/**
* @brief Debug MCU
*/
typedef struct
{
__IO uint32_t IDCODE; /*!< MCU device ID code, Address offset: 0x00 */
__IO uint32_t CR; /*!< Debug MCU configuration register, Address offset: 0x04 */
__IO uint32_t APB1FZ; /*!< Debug MCU APB1 freeze register, Address offset: 0x08 */
__IO uint32_t APB2FZ; /*!< Debug MCU APB2 freeze register, Address offset: 0x0C */
}DBGMCU_TypeDef;
2020-12-15 07:27 AM
And do those actually need to be volatile either? I think you're working this problem in the wrong direction.
A bug would be a situation where something changed outside of program control/flow and wasn't marked as volatile.
The blanket __IO in the structures avoids a lot of register level evaluation and maintenance on the library maintainers part, some of whom might not have a particularly strong understanding of the exact HW interactions at a bit/register level.
2020-12-16 12:25 AM
Thanks. I got confused why particularly these register wasn't defined as volatile. But I understand now. For non-volatile it reads it at least once but than maybe no more. And for volatile it always reads it again before evaluating.