cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F7 JPEG decoder, 16-bit DQT JPEGS

DMame.1
Associate

Hello,

I'm developing a HAL-based software running on STM32F778AI MCU. The software uses the hardware JPEG decoder in DMA mode.

It decodes 'classical' JPEG images that have 8-bit DQTs without an issue.

But if a JPEG's the precision of the quantization table is set to 1 and its luminance table defined with 16-bit values, then the JPEG decoder fails.

Is there a nice way to make F7's JPEG decoder work on JPEGs with 16-bit DQTs?

0 REPLIES 0