cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMx LTDC version 5.6.7 produce code with 1 Layer, version 6.0 produce code for 2 layers even if set 1. Is this a bug?

FMarr.2
Associate III

Open STM32H7BWorkshop2020 STM32H7B3I-DK.ioc first do not migrate, and generate code. Then migrate and generate code. Then check content of static void MX_LTDC_Init(void)

2 REPLIES 2
Khouloud ZEMMELI
ST Employee

Hello @Community member​ ,

Normally this issue has been fixed with the 6.1.0 CubeMX version, can you please check with it ?

Thanks, Khouloud

FMarr.2
Associate III

Hi, thanks for reply.

I am currently using 6.1.1 but i did not check if fixed. Just modified the produced code removing manually the second layer.

Regards