cancel
Showing results for 
Search instead for 
Did you mean: 

Inconsistency between STM32CubeIDE v1.5 and v1.4 on Mac

JZhan.9
Associate II

Hi,

On Mac, I am using Nucleo-H743ZI2. Leaving everything else as default. When using CubeIDE v1.4, I am able to set PA4 as a DAC1_out and use Timer1 Trigger Out event as the trigger. But after upgrading to v1.5, Trigger menu only starts from Timer2 Trigger Out event.

I have attached the screenshot of v1.5 as well.

Is this a bug or a feature?

0693W000005CEMZQA4.png 

Thank you very much.

0 REPLIES 0