cancel
Showing results for 
Search instead for 
Did you mean: 

Cube programmer api or one of its dependencies missing, java error. cube IDE version 2.6.0

MBhar.2
Associate II

i am getting the same error with cube programmer version 2.5.0

i am using windows 7 32 bit.

Java JRE build 1.8.0_271-b09

i have tried all the solutions given in previous posts but couldnt get past this.

the user manual of cube programmer 2.6.0 says :

"There is no need to install any Java™ SE Run Time Environment since version 2.6.0. The

STM32CubeProgrammer runs with a bundled JRE available inside the downloaded

package and no longer with the one installed on your machine."

please help

2 REPLIES 2
Houda GHABRI
ST Employee

Hi @MBhar.2​ ,

As your windows is 32 bit ,can you please verify that STM32CubeProgrammer 2.6.0 downloaded installed is 32bit version also?

Houda

MBhar.2
Associate II

Hi @Houda GHABRI​ 

thank you for the reply.

yes i believe i have the 32 bit version.

i have the zip file

en.stm32cubeprg-win32_v2-6-0.zip

and setup file name is mentioned as

SetupSTM32CubeProgrammer_win32.exe