cancel
Showing results for 
Search instead for 
Did you mean: 

Hi, I want to protect(over v and i) a 2.5hp AC motor with stm8 and BTA41 triac. I need to prevent triac to turn off when motor is in the off state because a light load series with motor, which control the water pressure and turns the motor on and off.

pghal.1
Associate

BTA41 has holding current of 80mA. Thank you all.

0 REPLIES 0