cancel
Showing results for 
Search instead for 
Did you mean: 

When inserting the CAN_Send block in Simulink I get the warning "configuration must be done first". I added the config file from STMCube which works fine with the GPIOs and ADC. Only the CAN_Block triggers the warning. STMCube 6.1.0 & patches installed.

MRau.1
Associate

Is there a possibility to write a S-function and use it instead of the can_block?

I am using STM32F103C8Tx

Thank you for answers

0 REPLIES 0